cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFXHAL::flushFrameBuffer() is only called once after the first OSWrappers::signalVSync(). What am I missing?

MKiss.1
Associate II

Considering existing posts and instructions in the documentation, I can't manage the framework to call flushFrameBuffer() regularly after a vsync.

The main issue is that TouchGFXHAL::flushFrameBuffer() is only called once after the first OSWrappers::signalVSync() (and never again). I've deleted all display drivers and checked with a breakpoint that is only hit once in TouchGFXHAL::flushFrameBuffer(). OSWrappers::signalVSync() is triggered by a button and an external interrupt callback. All code that I added is attached. The board is a F303RE Nucleo. Settings of TouchGFX see below.

Many thanks for considering my request.

Sync wrapper. Breakpoint hit on each button press.

0693W000008GH4sQAG.png 

Callback on button press. Calls the wrapper function from above.0693W000008GH03QAG.png 

Breakpoint gets hit.0693W000008GH6PQAW.pngBreakpoint only hit on first button press!0693W000008GH6jQAG.pngTouchGFX settings.0693W000008GH6oQAG.png

1 ACCEPTED SOLUTION

Accepted Solutions
N. SANTINI
ST Employee

Hi,

Indeed, the flushFrameBuffer function is called by the TouchGFX library only when something has changed in the frame buffer.

Best regards,

Nicolas

View solution in original post

9 REPLIES 9
MM..1
Chief II

When you setup Custom Interfaces, you need write full support for graphics refresh. Read demo for SPI displays, or change your config ...

I'm aware of that. But all of the transmission (e.g. start of SPI DMA) would be located in TouchGFXHAL::flushFrameBuffer(), which is not executed (more precisely: it is only executed once after the very first vsync). That's why I have deleted all display driver code for this forum.

MM..1
Chief II

Callback on button press. Calls the wrapper function from above.0693W000008GH03QAG.png 

check if gpio exti for you work once or more

The LED toggling works as expected. Also, a breakpoint in OSWrappers::signalVSync() is hit on each button press. 

OK then try read here TouchGFX custom driver- vsync problem

maybe helps

Oh, dear. Maybe I was thinking completely wrong. As the display has its own framebuffer: Is flushFrameBuffer() called when nothing has changed in the touchGFX framebuffer? I'll test it shortly.

N. SANTINI
ST Employee

Hi,

Indeed, the flushFrameBuffer function is called by the TouchGFX library only when something has changed in the frame buffer.

Best regards,

Nicolas

MKiss.1
Associate II

@N. SANTINI​ Thank you for providing clarification.

Kind regards,

Meinhard 

@N. SANTINI​  Thank you for providing clarification.

Kind regards,

Meinhard