2022-08-29 02:34 AM
We are evaluating TouchGFX and its performance in details. Can anyone please provide some technical details regarding below criteria, that would be appreciated.
Thanks in Advance
2022-08-29 03:03 AM
2022-08-29 06:41 AM
Hi @MM..1
Thanks for the prompt response.
Can you please explain in details?
UI reusability
E.g. In case if I've used button and I want to update the image of that button from rectangle to round in shape, then is it possible without change?
Graphics Resolution Scaling
How to make it possible? Do I need to update in the CubeMX project?
Custom Animation Support
At what level we can create an animation? Is it like complex or minimal?
Use Sketch Assets Directly (Intelligent reimport of sketch assets)
For this, there are direct sketch file available for graphics like icon pack, multiple small images file etc. So is it possible to import that sketch file direct into touchGFX instead of single asset and use those assets from one file?
Web Engine in UI
For support HTML web browser
Thanks
2022-08-29 07:00 AM
For your first 3 question in detail , designer is created for simple touch engine create, minimal coding required. But when you start over prepared design coding, you can handle this question.
Sketchs as you describe and Web isnt supported.
2022-08-29 07:09 AM
If you've been tasked with evaluating this platform, evaluate it.
It's a free product, and consequently you can expect to carry your own support costs.
Watch some of the tutorial videos or seminar materials.