cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX: Query for technical details

maulesh
Associate II

We are evaluating TouchGFX and its performance in details. Can anyone please provide some technical details regarding below criteria, that would be appreciated.

  1. UI reusability(means is it possible to modified the UI assets of already created UI)
  2. Graphics Resolution Scaling (in term of using the different resolution display in the same project, changes needs to be done)
  3. Custom Animation Support
  4. Use Sketch Assets Directly (Intelligent reimport of sketch assets)
  5. Web Engine in UI
  6. Cyber Security for data protection

Thanks in Advance

4 REPLIES 4
MM..1
Chief III
  1. Yes & No based what you mean
  2. none if your code dont handle it
  3. Yes
  4. ???
  5. none
  6. no part of TGFX

Hi @MM..1​ 

Thanks for the prompt response.

Can you please explain in details?

UI reusability

E.g. In case if I've used button and I want to update the image of that button from rectangle to round in shape, then is it possible without change?

Graphics Resolution Scaling

How to make it possible? Do I need to update in the CubeMX project?

Custom Animation Support

At what level we can create an animation? Is it like complex or minimal?

Use Sketch Assets Directly (Intelligent reimport of sketch assets)

For this, there are direct sketch file available for graphics like icon pack, multiple small images file etc. So is it possible to import that sketch file direct into touchGFX instead of single asset and use those assets from one file?

Web Engine in UI

For support HTML web browser

Thanks

For your first 3 question in detail , designer is created for simple touch engine create, minimal coding required. But when you start over prepared design coding, you can handle this question.

Sketchs as you describe and Web isnt supported.

If you've been tasked with evaluating this platform, evaluate it.

It's a free product, and consequently you can expect to carry your own support costs.

Watch some of the tutorial videos or seminar materials.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..