cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX keyboard with password

Maximiliano
Senior

Hello to all,I am working on a stm32h745i-disk project that uses keyboard and I would like to hide the characters in the password field.

how can I do it? i.e. I don't understand when you press a key on the keyboard where do you type so that it is shown above the keyboard before you hit ok and it is passed to the GUI with “Unicode::strncpy(ContrasenaBuffer, keyboard.getBuffer(), CONTRASENA_SIZE);”

The video guide I used was:

https://www.youtube.com/watch?v=Tkz9099a7a4

testing and trying to understand the keyboard related files I could only hide them once you hit ok and they show up in the GUI using two buffers where one is filled with “*”.

 

I would like to do something similar to the video (minute 5:38) https://www.youtube.com/watch?v=0--7qFmWZMQ

but in my touchGFX code and later add a button to show the password if I want to but I guess I can do that later if I can solve this.

 

I share my View.cpp and the keyboard thing.please ignore Login_inicioView::Validacion_usuario() as it is something for the future.

Thanks.

 

16 REPLIES 16

thanks@Marc_LM 

If I think I can solve that, thinking about it, your idea gave me an idea hehe ,

that the button calls a function that updates the text with a buffer or the other.

 

I'm currently working with two buffers only I have to fix a small detail

and that is that the function that @GaetanGodart  passed me is also affected by other keys pressed that are no

I can't avoid the execution of that part of the code because I don't know what the value of that

of code because I don't know what value has the variable “keyChar” when that key is pressed

(I guess that makes the problem I'm having).

what problem is it? well when I press delete or shift whatever I type then on the keyboard is not saved anywhere and if I delete it is deleted.

and if I delete it deletes one position less than the pressed ones.

 

I am not sure what is going on but the text that is typed with keyboard that does not use the gaetan function does not have that problem so my only assumption that the problem is that, that function is called by pressing any key but if you press shift or delete several times it is only executed once keyPressedhandler while the function corresponding to delete or change to lowercase / uppercase if it continues running as many times as you press the corresponding key regardless of whether it is pressed continuously or after another key.

but the buffer will be corrupted or something and does not save any extra key presses after that action.

GaetanGodart
ST Employee

Hello @Maximiliano and @Marc_LM ,

 

Indeed, it is not possible to change font for a single textArea at runtime.

 

Maximiliano, you can use the touchgfx_printf() method to print the value of the key in a console when running the simulator.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

thank you very much @GaetanGodart ,

With this I was able to move forward little by little to achieve my goal. again thanks for the follow up.

 

@Marc_LM thanks also.

Hello @Maximiliano ,

 

I am glad you were able to achieve your desired result!

Don't hesitate if you have other TouchGFX related question. :smiling_face_with_smiling_eyes:

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)
Marc_LM
Associate III

@Maximilianodid you find a way to have passwords in text boxes?

I am about to test a method of deriving a TextAreaWithWildcardBase like the flexButton with the "*style" composed templated classes.

Hi @Marc_LM sorry for the delay.

Yes,I was able to solve it.

I don't remember well now but I made two buffers where one typed ****** and the other the password. then I added a button which if pressed showed one buffer or the other in the text on the screen.

What I had to take into account is that in the keyboard function if I pressed any key that was not a character (e.g. shift or upper case) it failed and I could not type another character, so I used the following to check before if it was a character or not by giving an ascii code range.

 

void CustomKeyboard::keyPressedhandler(Unicode::UnicodeChar keyChar) { if(modo_password == 1 && keyChar >= 0x20 && keyChar <= 0x7E) { ContrasenaBuffer2[pos_pswrd]=keyChar; pos_pswrd++; // Replace the actual key character with '*' keyChar = '*'; //touchgfx_printf(keyChar); // Add the '*' character to the buffer uint16_t pos = keyboard.getBufferPosition()-1; if (pos < BUFFER_SIZE - 1) { buffer[pos] = keyChar; keyboard.setBufferPosition(pos + 1); } } else{ } }

I hope I can help you.

 

 

Thanks for the confirmation.
I did tried exploring overloading the "TextAreaWithWildcardBase::draw" to hide the wildcards but that function is not virtual.

I finished testing my implementation yesterday with double buffers.
I guess Gaetan's suggestion was the most reasonable compromise.