cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX display orientation and layout rotation at 180 and 270

ARM_and
Associate III

We have a 480W 800H  TFT display that TouchGFXDesigner can nicely display in landscape mode instead of portrait.

The trouble is that the device UI is now upside down. TouchGFXDesigner doesn't seem to accept other display rotations such as 180 and 270. Correct?

 

The designer does allow for the text to be rotated 180 which would look correct on our display. But that has other consequences.

Has anyone else had this issue?

 

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
GaetanGodart
ST Employee

Hello @ARM_and ,

 

We do not support that feature directly in TouchGFX because the display should have that functionality already (to flip the display at least).
So with just 0 and 90 degree plus the display's driver, you can get to 180 or 270.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

View solution in original post

7 REPLIES 7
GaetanGodart
ST Employee

Hello @ARM_and ,

 

We do not support that feature directly in TouchGFX because the display should have that functionality already (to flip the display at least).
So with just 0 and 90 degree plus the display's driver, you can get to 180 or 270.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

Thank you @GaetanGodart.  I see that there are other posts about this as well: https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/dsi-display-is-mirrored/td-p/733566 

 

Regards,

-A

amb
Senior

There is a custom widget on forum,https://community.st.com/s/question/0D50X0000A1lVxs/repost-change-lcd-orientation-in-180-degree

I tried it in my project,It is working,but cost very long time,about 10ms(my screen is 320*240,rgb565,160Mhz cpu),So I changed it a bit.Now it uses 5ms turn screen upside down.here is my  changed part.but your screen is 800*480,the time maybe expand several times.

// 16 Bit implementation

virtual void draw(const touchgfx::Rect& invalidatedArea) const

{

uint16_t *framebuffer = touchgfx::HAL::getInstance()->lockFrameBuffer();

 

const uint32_t total_pixels = 320 * 240;

uint32_t *buffer_32 = (uint32_t *)framebuffer; // 转换为32位指针

const uint32_t nblocks = total_pixels / 2; // 32位块的数量

uint32_t *start = buffer_32;

uint32_t *end = buffer_32 + nblocks - 1;

uint32_t a;

while (start < end) {

// 读取两个32位块(各包含2个像素)

a = *start;

// 交换每个块内的两个像素(高16位和低16位互换)

*start = ((*end) >> 16) | ((*end) << 16);

*end = (a >> 16) | (a << 16);

start++;

end--;

}

 

touchgfx::HAL::getInstance()->unlockFrameBuffer();

}

 

ARM_and
Associate III

It might be helpful to add that little bit about "0 and 90 degree plus the display's driver covering the rest" in the documentation.

Confirming that adding the commands for MADCTRL and SDIR  to the glass init sequence rotates it 180.

Hi Gaetan,

Unfortunatly a lot of Displays with simple RGB888 TTL interface do not have the possibility to rotate or flip the Display (for example the RockTech Display used in the STM32H735G-DK!).

Please consider this for a future release.

best regards

Martin

@MHoll.2  the LCD may even support it (see below) but the LCD SPI pins are just not present on the ever popular 40-pin FPC ribbon which makes things difficult.

 

ARM_and_1-1753967439542.png

 

 

 

I have a st7272a driver LCD,It  has Vdir and Hdir.I tried to change these two bits,but have no use.