cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX display int16_t value

khanhcong861989
Associate III

Dear all!

I 'm handle a project using ST7735 with flatform is TouchGFX, in Set2 is ADC value from POT( from -85 to -55) i debug and monitor on Keil C, the value is correct, When i display it to Screen the value is "-?5", i don't how to fix it, please share me why and how to fix.

1 ACCEPTED SOLUTION

Accepted Solutions
ferro
Senior III

Hi @khanhcong861989 . Force including of characters from the font with '0x00-0xff'

[Texts > Typographies > Default]

ferro_0-1730400888792.png

 

View solution in original post

4 REPLIES 4
ferro
Senior III

Hi @khanhcong861989 . Force including of characters from the font with '0x00-0xff'

[Texts > Typographies > Default]

ferro_0-1730400888792.png

 

ferro
Senior III

And update the battery text area

 

 

void Screen1View::setvaluetoscreen( int BAT_Val, int16_t pressure, int16_t set2, bool pump1_sta,bool valve1_sta,int16_t temp_pressure)
{
    Unicode::snprintf ( textArea7Buffer, TEXTAREA8_SIZE, "%d", BAT_Val);
    textArea7.invalidate ();
}

 

 

 

ferro_0-1730402448502.png

 

khanhcong861989
Associate III

many thank @ferro issue was fixed, i can display set2. 1 more. may i add new fonts to touchGFX, how can i do it

@khanhcong861989glad to hear.

 

"may i add new fonts"

Yes you can. With GfxDesigner closed, copy font to ./assets/fonts and it will be in the list of available fonts of GfxDesigner.