2024-10-30 05:43 PM
Dear all!
I 'm handle a project using ST7735 with flatform is TouchGFX, in Set2 is ADC value from POT( from -85 to -55) i debug and monitor on Keil C, the value is correct, When i display it to Screen the value is "-?5", i don't how to fix it, please share me why and how to fix.
Solved! Go to Solution.
2024-10-31 11:57 AM - edited 2024-10-31 11:58 AM
Hi @khanhcong861989 . Force including of characters from the font with '0x00-0xff'
[Texts > Typographies > Default]
2024-10-31 11:57 AM - edited 2024-10-31 11:58 AM
Hi @khanhcong861989 . Force including of characters from the font with '0x00-0xff'
[Texts > Typographies > Default]
2024-10-31 12:19 PM - edited 2024-10-31 12:22 PM
2024-10-31 06:15 PM
many thank @ferro issue was fixed, i can display set2. 1 more. may i add new fonts to touchGFX, how can i do it