2023-03-31 12:00 AM
last time also this problem was occured so I installed it again after that it run for some days now again the problem has occured.
When I open Touchgfx one msg come
Sorry - something unexpected has happened which caused an error to occur in the Designer.
For more information, see the log file located at: C:\Users\Kaushal\AppData\Roaming\TouchGFX-4.21.3\TouchGFXDesigner.log
Please someone help to give the solution of it.
Solved! Go to Solution.
2023-04-12 1:21 AM
2023-04-12 11:57 PM
Hello,
This file looks empty or erroneous, did you modify it before sharing it ?
/Yoann
2023-04-13 9:09 PM
No I didn't I send it to you once again
2023-04-13 9:10 PM
2023-04-13 9:11 PM
2023-04-13 10:00 PM
2023-04-13 11:44 PM
When you open this file in a text editor, what do you see ?
/Yoann
2023-04-14 2:28 AM
Actually the touchgfx doesn't open so I can't open any of these files.
But I didn't modify it because I can't do it.
2023-04-14 3:27 AM
I mean, when you right click on it and open it with Notepad.
/Yoann
2023-04-14 9:57 PM