2023-04-25 2:06 AM - edited 2023-11-20 7:12 AM
I just installed TouchGFX Designer 4.21.3 yesterday and now whenever I try to run simulator or run target I get these errors:
gcc/makefile_cm7:403: recipe for target 'CM7/TouchGFX/build/STM32H745I_DISCO/CM7/TouchGFX/gui/src/main_screen/mainView.o' failed
make[3]: *** [CM7/TouchGFX/build/STM32H745I_DISCO/CM7/TouchGFX/gui/src/main_screen/mainView.o] Error 1
make[3]: Leaving directory 'c:/Users/o.sang/Documents/TouchGFX/MyApplication_3'
gcc/makefile_cm7:368: recipe for target 'generate_assets' failed
make[2]: *** [generate_assets] Error 2
make[2]: Leaving directory 'c:/Users/o.sang/Documents/TouchGFX/MyApplication_3'
makefile_cm7:49: recipe for target 'all' failed
make[1]: *** [all] Error 2
make[1]: Leaving directory 'C:/Users/o.sang/Documents/TouchGFX/MyApplication_3/gcc'
../../gcc/Makefile:10: recipe for target 'flash' failed
make: *** [flash] Error 2
Failed
FailedI check other posts in the ST community but there were no answers to solve my problem. I used STM32 Programmer and was able to connect with my STM32H745I-disco board, so ST-Link is working fine!
This is my configuration for the build:
Could someone please help solve this problem?
2023-04-27 7:40 AM
@Osman SOYKURT
Log from Run Simulator:
Run Simulator
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
.cproject file: ../../STM32CubeIDE/CM7/.cproject
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.project
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.cproject
Done
Compile
make -f simulator/gcc/Makefile -j8
Reading ./application.config
Reading ./target.config
Compiling gui/src/screen1_screen/Screen1View.cpp
gui/src/screen1_screen/Screen1View.cpp:2:10: fatal error: stm32h7xx_hal.h: No such file or directory
#include "stm32h7xx_hal.h"
^~~~~~~~~~~~~~~~~
compilation terminated.
generated/simulator/gcc/Makefile:196: recipe for target 'build/MINGW32_NT-6.2/gui/src/screen1_screen/Screen1View.o' failed
make[2]: *** [build/MINGW32_NT-6.2/gui/src/screen1_screen/Screen1View.o] Error 1
generated/simulator/gcc/Makefile:155: recipe for target 'generate_assets' failed
make[1]: *** [generate_assets] Error 2
simulator/gcc/Makefile:32: recipe for target 'all' failed
make: *** [all] Error 2
Failed
Failed
2023-04-27 7:41 AM
Run Target works!
Had to removed all the compiling and generating lines because post was too long and won't let me post it...
Run Target
Generate
Done
Generate Assets
make -f simulator/gcc/Makefile assets -j8
Reading ./application.config
Reading ./target.config
Done
Post Generate
touchgfx update_project --project-file=simulator/msvs/Application.vcxproj
Done
Post Generate Target
touchgfx update_project
.cproject file: ../../STM32CubeIDE/CM7/.cproject
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.project
Writing STM32CubeIDE project file: ../../STM32CubeIDE/CM7/.cproject
Done
Compile
make -f ../../gcc/Makefile clean && make -f ../../gcc/Makefile -j8
make -C C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc/ -f makefile_cm4 clean
make[1]: Entering directory 'C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc'
make[2]: Entering directory 'c:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2'
Cleaning: STM32H745I_DISCO
make[2]: Leaving directory 'c:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2'
make[1]: Leaving directory 'C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc'
make -C C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc/ -f makefile_cm7 clean
make[1]: Entering directory 'C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc'
make[2]: Entering directory 'c:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2'
Cleaning: STM32H745I_DISCO
make[2]: Leaving directory 'c:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2'
make[1]: Leaving directory 'C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc'
make: 'Makefile' is up to date.
Done
Flash
make -f ../../gcc/Makefile flash
make -C C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc/ -f makefile_cm4 flash
make[1]: Entering directory 'C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc'
make[2]: Entering directory 'c:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2'
make[3]: Entering directory 'c:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2'
Memory Programming ...
Opening and parsing file: target.hex
File : target.hex
Size : 524.46 KB
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Erasing memory corresponding to segment 1:
Erasing internal memory sectors [0 1]
Erasing memory corresponding to segment 2:
Erasing external memory sectors [0 2]
Download in Progress:
±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0%
ÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛÛ 96%ÛÛ 100%
File download complete
Time elapsed during download operation: 00:00:04.410
Hard reset is performed
make[2]: Leaving directory 'c:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2'
make[1]: Leaving directory 'C:/Users/o.sang/Documents/TouchGFX/LED_Toggling_2/gcc'
Done
Done
2023-04-27 7:43 AM
@Pavel A. See reply below now, I hope this answers your question.
I don't know why I keep getting error at either run target or simulation from time to time on each different project.
2023-05-02 6:25 AM
@Osman SOYKURT any success on finding why this error occurs on my side?
Also to answer your question, I am using Windows 10. I have also attached the log from AppData\Roaming
2023-05-02 7:22 AM
Problem appears in touchgfx example as well. Trying to run target for Smart Home example on my STM32H745I Disco board but it's giving out recipe for target '_clean_' failed and so on...