cancel
Showing results for 
Search instead for 
Did you mean: 

touchgfx breaks ethernet connection

wonderFine
Associate II

hello,

I customized a board with stm32h743iit6 for HMI application, the main hardware features available on the board are RMII ethernet, 32bit SDRAM and LTDC RGB565 interface. Below is the board picture.

微信图片_20250104114456.jpg

A test MDK keil project is generated by cubemx to test ethernet communication, freertos and lwip are enabled.

Packet loss ratio is zero even for a very long time test, and tcp echo application works fine.

wonderFine_0-1735963299350.png 

 

wonderFine_2-1735965166074.png

 

But packet loss ratio rises to about 0.1% when touchgfx added to the project. if interacting with touchgfx screen, ethernet connection will break immediately,while  touchgfx still works correctly.

I have tried to improve priority and increase stack size of lwip thread, still can't solve it.

what did I miss?

here is the cubemx config file.

0 REPLIES 0