cancel
Showing results for 
Search instead for 
Did you mean: 

TouchGFX 8bpp color format

VLau
Associate III

Hey!

I'm having wrong colors issue when drawing shapes with 8 bpp color format. It's clean simulator project with only color format settings changed. How to fix that?

Images attached.

Thanks

3 REPLIES 3
MM..1
Chief II

Shapes need canvas buffer to draw. Try set custom value when click on screen properties

VLau
Associate III

I set the maximum Canvas buffer size without effect

VLau
Associate III

Just tried to make the same project in TGFX Designer 4.16 - and it worked. Those shapes are drawn as expected.

In 4.17 it doesn't.

My project is written with 4.17 - I don't think there's back compability, so I need some workaround.