2023-03-28 7:06 AM
hi guys,
I created a project, which was done with touchgfx 4.20.0. After the software has a new version 4.21.3, I use it to open the old version. After generating the code, a compilation error occurs, and the prompt is as follows
h7b0_vbt_touchgfx\h7b0_vbt_touchgfx.axf: Error: L6218E: Undefined symbol touchgfx::paint::tearDown() (referred from painterrgb565.o).
I can't find the reason, can you help me to find the reason? Thank you for your support.
2023-03-30 2:44 AM
Hello @victor.wu,
Did you think about regenerating code on TouchGFX 4.21.3 ?
Also, did you use CubeMX ?
/Yoann
2023-03-30 3:11 AM
Yes, I thought of this possibility, so I used cubemx to regenerate the code, and the compilation passed, but a new problem appeared again, and the display was sometimes blurred, so I have to continue to troubleshoot the problem, thank you for your answer