User Activity

hi guys,  I created a project, which was done with touchgfx 4.20.0. After the software has a new version 4.21.3, I use it to open the old version. After generating the code, a compilation error occurs, and the prompt is as followsh7b0_vbt_touchgfx\h7...
hi guys,  I created a project, which was done with touchgfx 4.20.0. After the software has a new version 4.21.3, I use it to open the old version. After generating the code, a compilation error occurs, and the prompt is as followsh7b0_vbt_touchgfx\h7...
sld_809_g070rbt\sld_809_cnt_g070rbt.axf: Error: L6286E: Relocation #REL:7 in tx_timer_initialize.o(.text._tx_timer_initialize) with respect to Veneer$$LitPool. Value(0xfffff21f) out of range(0 - 0xff) for (R_ARM_THM_PC8)sld_809_g070rbt\sld_809_cnt_g0...
The method is as follows:1. First, set the flash option byte to force boot from the main flash.2. Set the read protection level to level 1.After this setting, the st-link tool will no longer be able to connect to the chip, which is equivalent to losi...
Using threadx rtos, spi is written to st7796 rbg565 480*320, the interface display is normal during initialization, but it is abnormal when the widget is refreshed in handletickevent