cancel
Showing results for 
Search instead for 
Did you mean: 

Touch Display getting flicker when data is getting updated through TouchGFX task

JJhin.1
Senior II

Hello Friends.

 

Now i have started working on bigger display with TouchGFX Custom Boards. Im using 10.1 inch 1024x600 touch display. using QUADSPI,SDRAM, FMC and LTDC.

 

Through TouchGFX Designer i taken one backgoround image, one Text Area buffer and one Digital clock. when im not updating digital clock data and text area im  getting proper display.

Nor.jpeg

but when i starts updating digital clock in void screenView::handleTickEvent() then my display starts flickering and white lines appearing on display.

FL.jpegFL2.jpeg

 

my LTDC configuration:

void MX_LTDC_Init(void)
{

  /* USER CODE BEGIN LTDC_Init 0 */

  /* USER CODE END LTDC_Init 0 */

  LTDC_LayerCfgTypeDef pLayerCfg = {0};

  /* USER CODE BEGIN LTDC_Init 1 */

  /* USER CODE END LTDC_Init 1 */
  hltdc.Instance = LTDC;
  hltdc.Init.HSPolarity = LTDC_HSPOLARITY_AL;
  hltdc.Init.VSPolarity = LTDC_VSPOLARITY_AL;
  hltdc.Init.DEPolarity = LTDC_DEPOLARITY_AL;
  hltdc.Init.PCPolarity = LTDC_PCPOLARITY_IPC;
  hltdc.Init.HorizontalSync = 40;
  hltdc.Init.VerticalSync = 9;
  hltdc.Init.AccumulatedHBP = 200;
  hltdc.Init.AccumulatedVBP = 29;
  hltdc.Init.AccumulatedActiveW = 1224;
  hltdc.Init.AccumulatedActiveH = 629;
  hltdc.Init.TotalWidth = 1384;
  hltdc.Init.TotalHeigh = 659;
  hltdc.Init.Backcolor.Blue = 0;
  hltdc.Init.Backcolor.Green = 0;
  hltdc.Init.Backcolor.Red = 0;
  if (HAL_LTDC_Init(&hltdc) != HAL_OK)
  {
    Error_Handler();
  }
  pLayerCfg.WindowX0 = 0;
  pLayerCfg.WindowX1 = 1024;
  pLayerCfg.WindowY0 = 0;
  pLayerCfg.WindowY1 = 600;
  pLayerCfg.PixelFormat = LTDC_PIXEL_FORMAT_RGB888;
  pLayerCfg.Alpha = 255;
  pLayerCfg.Alpha0 = 0;
  pLayerCfg.BlendingFactor1 = LTDC_BLENDING_FACTOR1_PAxCA;
  pLayerCfg.BlendingFactor2 = LTDC_BLENDING_FACTOR2_PAxCA;
  pLayerCfg.FBStartAdress = 0xD0000000;
  pLayerCfg.ImageWidth = 1024;
  pLayerCfg.ImageHeight = 600;
  pLayerCfg.Backcolor.Blue = 0;
  pLayerCfg.Backcolor.Green = 0;
  pLayerCfg.Backcolor.Red = 0;
  if (HAL_LTDC_ConfigLayer(&hltdc, &pLayerCfg, 0) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN LTDC_Init 2 */

  /* USER CODE END LTDC_Init 2 */

}

 

my FMC configuration:

void MX_FMC_Init(void)
{
  /* USER CODE BEGIN FMC_Init 0 */

  /* USER CODE END FMC_Init 0 */

  FMC_SDRAM_TimingTypeDef SdramTiming = {0};

  /* USER CODE BEGIN FMC_Init 1 */

  /* USER CODE END FMC_Init 1 */

  /** Perform the SDRAM1 memory initialization sequence
  */
  hsdram1.Instance = FMC_SDRAM_DEVICE;
  /* hsdram1.Init */
  hsdram1.Init.SDBank = FMC_SDRAM_BANK2;
  hsdram1.Init.ColumnBitsNumber = FMC_SDRAM_COLUMN_BITS_NUM_8;
  hsdram1.Init.RowBitsNumber = FMC_SDRAM_ROW_BITS_NUM_12;
  hsdram1.Init.MemoryDataWidth = FMC_SDRAM_MEM_BUS_WIDTH_16;
  hsdram1.Init.InternalBankNumber = FMC_SDRAM_INTERN_BANKS_NUM_4;
  hsdram1.Init.CASLatency = FMC_SDRAM_CAS_LATENCY_3;
  hsdram1.Init.WriteProtection = FMC_SDRAM_WRITE_PROTECTION_DISABLE;
  hsdram1.Init.SDClockPeriod = FMC_SDRAM_CLOCK_PERIOD_2;
  hsdram1.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;
  hsdram1.Init.ReadPipeDelay = FMC_SDRAM_RPIPE_DELAY_1;
  /* SdramTiming */
  SdramTiming.LoadToActiveDelay = 2;
  SdramTiming.ExitSelfRefreshDelay = 7;
  SdramTiming.SelfRefreshTime = 4;
  SdramTiming.RowCycleDelay = 6;
  SdramTiming.WriteRecoveryTime = 2;
  SdramTiming.RPDelay = 2;
  SdramTiming.RCDDelay = 2;

  if (HAL_SDRAM_Init(&hsdram1, &SdramTiming) != HAL_OK)
  {
    Error_Handler( );
  }

  /* USER CODE BEGIN FMC_Init 2 */
  FMC_Bank1_R->BTCR[0] &= ~FMC_BCRx_MBKEN;
  BSP_SDRAM_Init();
  /* USER CODE END FMC_Init 2 */
}

i dont have a idea whats going wrong with this display. if any one knows please help to resolve this issue.

8 REPLIES 8
PMerv.1
Associate II

If yours LTDC settings for display are correct, what about LTDC clock ? For 1024x600 you need at least freq around 50-60Mhz - see example bellow  - Riverdi 10.1" uses 57.92Mhz
image.png

JJhin.1
Senior II

hi @PMerv.1  thanks for replying. im using waveshares 10.1 Capacitive LCD Touch(D) display. i tried LTDC frquency from 20 MHz to 45 MHz its showing same. but when im increasing frequency above 45MHz its flickring even more. max frequnecy i tried is 59MHZ.

Strange, 745-DISCO (4.3" 480x272) uses LTDC clocks around 10Mhz, same kit but 5" 800x480 already needs around 20-30Mhz. And if you have even bigger resolution, you need higher LTDC clocks in principle....
Anyway, do you have some datasheet for that kind of LCD ? Is here already some LVDS -> RGB (LTDC) converter IO  (like Riverdi uses it for that big displays) ?
PS: my mistake in first reply: Riverdi 10.1 uses 1280x800 and 58Mhz, so  for 1024x600 + some LTDC  clock equation

PMerv1_0-1740556341109.png

 

JJhin.1
Senior II

as pr my display data sheet its supports 44.9 to 63 MHZ frequency. im refering this Data Sheet .

It seems your seetings is correct, anyway try to play with  h/v sync width (pdf says h: 1-140 /  v:1-20) )  + LTDC clocks between 40 - 70Mhz.
 + yes, it's LVDS display, so check your LVDS -> LTDC converter circuit

PMerv1_0-1740562305609.png

 

JJhin.1
Senior II

hii @PMerv.1  im playing with  play with  h/v sync width and LTDC clocks ... BTW what i need to check in LVDS to LTDC converter circuite?

PMerv.1
Associate II

Anyway, I've remember, I had similar problems with Riverdi 10 (see this video here https://k00.fr/RiverdiFLicker )
And my solution was to remove Riverdi TouchGFX RTOS task (in CubeMX)  and create/start it manually in my app manager as last task, and it was solved...

uint32_t TouchGFXStack[8192];  

/*****************************************************************************/
// Definitions for TouchGFXTask

const osThreadAttr_t TouchGFXTask_attributes = {
  .name = "TouchGFXTask",
  .cb_mem = &TouchGFXTcb,
  .cb_size = sizeof(TouchGFXTcb),
  .stack_mem = (void*)TouchGFXStack,
  .stack_size = sizeof(TouchGFXStack),
  .priority = (osPriority_t) osPriorityNormal,
};



// Start application's processes in defined order
// supervisor priority is osPriorityNormal

static void StartAppProcs(AppSuper * obj)     
{
  // execute tasks of application - MEP - oblsuha CAN Rx/Tx - 2ms loop
  ExecUfProc(ComManCreate(&comMan, comManStack, sizeof(comManStack)), osPriorityAboveNormal);
  while (!ComManIsRdy()) ufDelay(1);
  ExecUfProc(IoManCreate(&ioMan, ioManStack, sizeof(ioManStack)), osPriorityNormal);
  while (!IoManIsRdy()) ufDelay(1);

   // creation of TouchGFXTask
   osThreadNew(TouchGFX_Task, NULL, &TouchGFXTask_attributes);
   ufDelay(4);
}

// and Screen1View.cpp...
void Screen1View::handleTickEvent()
{
	HrTm tm = {0};

	hmi_cnt++;

	HrTimeToTm(RtcGet(), &tm);

    // clock modal window on ?
	if (modalClock.isVisible() == true)
	{
	  if ((hmi_cnt % 2) == 0) {
  	     anClk.setTime24Hour((int)tm.hour, (int)tm.min, (int)tm.sec);  // AnalogClock update
  	     digClk.setTime24Hour((int)tm.hour, (int)tm.min, (int)tm.sec);  // AnalogClock update
	  }
	  return;
	}
}




 About LVDS circuit: see this picture, t his is LVDS converter made by Riverdi. Differential tracks, equal lenghts of tracks....not easy to design it correctly..... But how to check it....I'don;t know....

Screenshot_2025-02-27-18-21-07-884_lockscreen.png

JJhin.1
Senior II

Removing TouchGFXTask from CubeMX and creating and starting it manually dosent working. its giving same out put