2022-12-15 1:06 PM
Hello,
I have written my 4 bit grayscale, 256x64 OLED driver using SPI, and I want to visualize my throttle position. The throttle value ranges between -100 and +100 where -100 means maximum deceleration and +100 the maximum acceleration. So far, I have successfully implemented the buffering technique in SPI, which is insanely fast and I can eliminate for loops. As the range increases from 0 to +100, a rectangle rises from the middle to upwards, and from 0 to -100 a rectangle increases from the middle to downwards. The previous version used for loops which were incredibly inefficient, so I started using buffers.
1 byte controls 2 pixels that have 16 brightness levels. 0xFF = 2 pixels at max brightness.
The problem is that if I decrease the size of the rectangle, it stays in the OLED's GDDRAM and they are not automatically written over with zeros.
I am using a bitmap array for the black and white rectangles. The size of the black and white rectangles is 6x56 pixels. In my case, one row is made up of 3 bytes, which means that every size has to be a multiple of 3. This is the value that I am passing into the writeData2 function.
So far I have made something to solve this but it doesn't really work properly. I split the incoming data into 3 cases, when the throttle is above zero, under zero and of course when it is zero. For the sake of simplicity I am showing the code only for the positive region.
The positive case uses 1 black and 1 white rectangle. I am controlling the start and end position of the rectangles and their size respectively.
At 0 throttle the black rectangle spans from 0 to the 30th row, and the white rectangle is just one line in 31.
At 100 throttle the black rectangle spans from 0 to 3 and the white rectangle from 4 to 31.
When the throttle value increases:
Now my code is working when I increase the value, but it doesn't decrease.
float throttlepos;
void teglalap2(int8_t gaz) { //-100 and + 100
if (gaz > 0) {
throttlepos = round(0.27f * gaz);
/* for debugging
watch = gaz;
feketerowend = 27 - throttlepos + 3;
feketesize = 90 - (throttlepos * 3);
feherrowstart = 27 - throttlepos + 4;
fehersize = 3 + (throttlepos * 3);
*/
setColAddr(0, 2);
setRowAddr(0, 27 - throttlepos + 3);
writeData2(black, 90 - (throttlepos * 3));
setColAddr(0, 2);
setRowAddr(27 - throttlepos + 4, 31);
writeData2(white, 3 + (throttlepos * 3));
}
}
Perhaps my calculations are wrong but I have been watching my variables and they look good.