2021-03-10 12:35 AM
The Additional Function of PB2 is LCD_VLCD2 in the data sheet, but the same pin is set to VLCD1 in dm00171429-evaluation-board-with-stm32l073vz and CubeMX.
Which is correct?
I will attach the corresponding image
Solved! Go to Solution.
2021-03-11 04:39 AM
Hello,
The datasheet is correct.
Regarding the reference manual, table "VLCD rail connections to GPIO pins" is wrong.
The error will be corrected in the next release.
Thanks again,
Imen
2021-03-10 01:35 AM
Hello @リョウスケ クボ
Thanks for your feedback, I'll check it then I'll get back to you.
Khouloud
2021-03-10 05:36 AM
Hello @リョウスケ クボ,
The correct one is LCD_VLCD2.
For documentation, I have reported the error to our team for correction.
For CubeMx,@Khouloud ZEMMELI Could you please fix this typo.
Thanks for your contribution.
Imen
2021-03-10 06:00 AM
Thank you @Imen GH for doing the check and for taking in charge the follow-up of the documentation issue, I confirm the issue from CubeMX side and it will be fixed.
Many thanks @リョウスケ クボ for raising these issues to our attention :)
Khouloud
2021-03-10 04:00 PM
Hello Imen GH (ST Employee), @Khouloud ZEMMELI (ST Employee)
Thnak you for answer my question.
Well then, Is generated code by CubeMX Wrong?
I want to use LCD Bias Selector with 1/3 Bias.
Please tell me how to fix it. (using the HAL library)
The Reference Manuals also look different.
I do not know whether it is sufficient that for any port in the correct setting.
2021-03-11 04:39 AM
Hello,
The datasheet is correct.
Regarding the reference manual, table "VLCD rail connections to GPIO pins" is wrong.
The error will be corrected in the next release.
Thanks again,
Imen
2021-08-19 03:07 AM
Hello @リョウスケ クボ ,
I'm back again to inform you that issue is now fixed, you can use the latest CubeMX version available on site :)
Khouloud