cancel
Showing results for 
Search instead for 
Did you mean: 

The shape widget setAngle

李林.1312
Associate II

When the shape widget is set to a new angle, it can not completely remove the disability from the previous angle. Is there a Bug or is there another way to solve this problem? Thank you!0693W000006EkexQAC.png0693W000006EkesQAC.png0693W000006EkenQAC.png

1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief II

Maybe workaround but try set visible false ... invalidate ... setAngle ... visible true ... invalidate

View solution in original post

3 REPLIES 3
MM..1
Chief II

Maybe workaround but try set visible false ... invalidate ... setAngle ... visible true ... invalidate

李林.1312
Associate II

0693W000006Em6nQAC.pngExactly�?​thanks, 👍

As if the setVisible function could be omitted?

when invalidate do job then yes you can omit