cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 QSPI memory compatibility

FDigi
Associate III

Hello everyone,

Recently I was navegating in the forum and I found a information that said STM32H7 had a list o QSPI memoty that are compatible with this micro controller.

I don't know if this information is true and as I am new in using STM micro controllers I would like to ask if all QSPI memory are compatible with the STM microcontroller. If this is not the case I would be most grateful if some one could recommend me a QSPI memory.

I planning to use this memory to store all the imagem from my TouchGFX Project.

1 REPLY 1

Care to cite the actual post?

I guess the primary sensitivity is to the CS timing. But used here with an assortment of Micron, Winbond and Macronix devices.

You're going to have to configure to match your board/part choices, and code a BSP to support a particular device.

If you're not game to write your own BSP and loader pick a part ST uses on a DISCO or EVAL board, with the same pins. The SOP2-16 300 mil footprint provides the most flexible part/bom choices.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..