cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F769I Discovery + TouchGFX 4.13 weird graphics issue

LMese.1
Associate II

Hello,

ALL TouchGFX examples and demos from TouchGFX Designer 4.13 templates have this graphics issue. The issue is quite randomic. For example, I compile, build and flash the demo, it runs ok, but after I un-plug and plug again the board it looks like the following. But not always, about twice on 3-4 attempts. Sometimes it starts ok. Pressing reset button sometimes helps and sometimes not. Please help. I'd like to use TouchGFX for our project, it is a very impressive product, but this strange issue is blocking. Thank you.

P.S. That's not a HW problem, other LTDC demos, including emWin, work just fine.

0690X00000BwdgBQAR.jpg

23 REPLIES 23
LMese.1
Associate II

up

Hi Martin :)

�� Nice to read, that meanwhile even YOU are a victim of buggy ST-firmwares and generators ��

Thanks for your honesty as ST employee ��

Michael K
Senior III

Bump - any updates on a new application template or fix for these graphical issues?

Seems that nobody cares about it. STM32F769I Disco doesn't work? Who cares, we will go ahead releasing newer cool DISCO boards and bugged firmware.