cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F769I and LCD

Ebun.1
Senior

Hello.

When using a 1024 × 768 resolution LCD with the STM32F769I,

Is performance bad?

Doesn't it move lightly?

If you have a proof result or other evidence, please post it.

Thank you.

7 REPLIES 7

Well the bandwidth is pretty close to the ceiling.

62.5 MHZ LTDC, 500 MHz DSI can get you 1024x768 @ 57 Hz 16-bpp

Probably want 32-bit memory width

Had it running via DSI-HDMI on STM32F769I-DISC1

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Martin KJELDSEN
Chief III

Depends on the complexity of your application. But 1024x768 is pushing it. 800x480 is already a stretch as it is if you want fast and fluent full screen transitions.

/Martin

Emerging display technologies are offering different display modules based on STM32F7s and H7s. One of them is running 1024*600, with a simple UI.

Here is a link to a video showing the 10,1" module, 1024*600, 16 bpp running a TOuchGFX application.

https://www.youtube.com/watch?v=mnShrk3nqCM&t

/Soren

Thank you for your reply.

Hello

When selecting the STM32F769I-DISCO template in TouchGFX

Color depth can be selected only 24bit.

How do I achieve 16bpp?

Hello Ebun1

For changing the color depth in the selected AT:

1: Browse code

2: Open project folder and and open the .ioc file which is a CubeMX file

3: Select additional software in CubeMX, set framebufferpixel format to desired color depth.

Br

Soren

Ebun.1
Senior

Hello.

Thank you for your reply.