cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F7508-DK : Blank screen after flashing TouchGFX GUI

Woula
Associate II

Hi,

I am trying to flash a single screen Touch GFX application on my STM32F7508-DK board but I got a blank screen.

Did anyone face that problem before ? What could be the solution ?

My actual configuration:

TouchGFX Designer 4.21.0

Thanks in advance!

3 REPLIES 3
Karl Yamashita
Lead III

Do you mean the STM32H750B-DK? Did you press the black reset button? I'm working on this board this very minute. Unlike other TouchGFX projects, this one does not start after being programmed from STM32CubeIDE until you reset it.

If smoke escapes your device, put the smoke back in. It'll still work as a conversation piece. If you find my answers useful, click the Accept as Solution button so that way others can see the solution.

No. I think they are different.

I did press the reset button many times but nothing had changed.

Even the examples are not displayed after being flashed. The screen remains blank.

Have you've checked to see if the External Loaders section has a memory device selected?

If smoke escapes your device, put the smoke back in. It'll still work as a conversation piece. If you find my answers useful, click the Accept as Solution button so that way others can see the solution.