cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G-DISCO, STM32CubeIDE_1.5.1, TouchGFX Designer 4.16.1, TouchGFX

ADębs.1
Senior

Witam posiadam płytę STM32F746G-DISCO. STM32CubeIDE_1.5.1, TouchGFX Designer 4.16.1. Ustawiłem zgodnie z: https://www.youtube.com/watch?v=12KXreXaLp0&t=3s mam błąd. Dlaczego?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

Could you add the TouchGFX tag to your post ? This will increase the visibility.

The video you shared is a bit outdated. You should create a project from TouchGFX Designer with the application template for the STM32F746 disco board, then generate code. In your project folder you just need to double click on the cubdeIDE project in the /STM32CubeIDE folder to work with this toolchain.

/Romain

View solution in original post

4 REPLIES 4
Romain DIELEMAN
ST Employee

Hi,

Could you add the TouchGFX tag to your post ? This will increase the visibility.

The video you shared is a bit outdated. You should create a project from TouchGFX Designer with the application template for the STM32F746 disco board, then generate code. In your project folder you just need to double click on the cubdeIDE project in the /STM32CubeIDE folder to work with this toolchain.

/Romain

How to do it?

I have uploaded a new video using the latest STM32CubeIDE 1.6.1 and TouchGFX 4.16.0

https://www.youtube.com/watch?v=Q-mfuzW6S-0

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source

Thank you. I watched. I'll check at the earliest opportunity.

greetings

Andrzej