cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F746G-DISCO, STM32CubeIDE_1.5.1, TouchGFX Designer 4.16.1, TouchGFX

ADębs.1
Senior

Witam posiadam płytę STM32F746G-DISCO. STM32CubeIDE_1.5.1, TouchGFX Designer 4.16.1. Ustawiłem zgodnie z: https://www.youtube.com/watch?v=12KXreXaLp0&t=3s mam błąd. Dlaczego?

1 ACCEPTED SOLUTION

Accepted Solutions
Romain DIELEMAN
ST Employee

Hi,

Could you add the TouchGFX tag to your post ? This will increase the visibility.

The video you shared is a bit outdated. You should create a project from TouchGFX Designer with the application template for the STM32F746 disco board, then generate code. In your project folder you just need to double click on the cubdeIDE project in the /STM32CubeIDE folder to work with this toolchain.

/Romain

View solution in original post

4 REPLIES 4
Romain DIELEMAN
ST Employee

Hi,

Could you add the TouchGFX tag to your post ? This will increase the visibility.

The video you shared is a bit outdated. You should create a project from TouchGFX Designer with the application template for the STM32F746 disco board, then generate code. In your project folder you just need to double click on the cubdeIDE project in the /STM32CubeIDE folder to work with this toolchain.

/Romain

How to do it?

I have uploaded a new video using the latest STM32CubeIDE 1.6.1 and TouchGFX 4.16.0

https://www.youtube.com/watch?v=Q-mfuzW6S-0

Tips and Tricks with TimerCallback https://www.youtube.com/@eebykarl
If you find my solution useful, please click the Accept as Solution so others see the solution.

Thank you. I watched. I'll check at the earliest opportunity.

greetings

Andrzej