cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F469I-DISCO. Screen using a custom container made-up for 16 checkbox, work in simulator but not in the hardware board.

Fran Marala
Associate III

Hi,

I'm developing an application using touchGFX Designer Version: 4.13.0, all is working correctly when you run Simulator in touchGFXDesingner tool, but when flashing in disco board the screen is fridge and I have to reset the system, again and again the same problem. I have tested that if I use only 4 checbox widget instead of 16 all is working properly, more than four return the same problem.

Waiting for your help

Regards

Fracncisco

2 REPLIES 2
Fran Marala
Associate III

Hi, I have tested tat in version 4.14 this bug is fixed

Fran Marala
Associate III

Sorry, unfortunately the problem still appear with version 4.14.

Attached below both the right option running is simulator and the bug running in dtn32469I-DISCO

0693W000004JEX8QAO.png

0693W000004JEZ4QAO.png

As you can see in the second picture, the screen referred is appearing from the west, but the screen is fridge a that point.