2020-04-12 4:22 PM
Hi!
Given the circumstances, I've finally found time to learn the STM32 dev environment. I have a STM32F769iDisco board.
I've successfully used TouchGFX v4.13.0 to start a new project with a simple interface (background and button). I can compile, simulate and run on target.
I've also been able to use CubeMX to open the ICO file and to modify board settings and then compiling & running using TouchGFX.
The issues begin when I try and debug using STM32CubeIDE. I open the project in a new workspace, build without errors, but when I try and run or debug I get an error.
In the console I get:
STMicroelectronics ST-LINK GDB server. Version 5.5.0
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Debugger connection lost.
Shutting down...
And a "Problem Occurred" Alert with the following error:
Error in final launch sequence:
Failed to execute MI command:
load C:\\TouchGFXProjects\\ScreenMaskingController\\STM32CubeIDE\\Debug\\STM32F769I_DISCO.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\ScreenMaskingController\\STM32CubeIDE\\Debug\\STM32F769I_DISCO.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\ScreenMaskingController\\STM32CubeIDE\\Debug\\STM32F769I_DISCO.elf
Error message from debugger back end:
Load failed
Load failed
The same project builds fine with TouchGFX but not via the IDE. Why?
Is there a way to change the IDE to use the same compiler/programmer settings TouchGFX is using?
Thanks.
2020-04-29 7:52 AM
Hi,
Are you still having this issue?
2020-12-20 6:33 AM
DMavr.1 how did you solve this isssue?
2021-01-14 6:14 AM
I encounter the same problem. Anybody an idea how to fix this?
2021-01-14 6:35 AM
Me too
2021-01-18 7:08 AM
Is an external flashloader configured for the project? These versions are pretty old now - what are your current toolchain versions?
Some of the ATs were missing flashloader configuration which would cause this. But should have been fixed.
2021-01-18 7:40 AM
I'm working with TouchGFX 4.16, STM32CubeIDE 1.51 (latest versions) on a NUCLEO-G071RB + X-NUCLEO-GFX01M1 board.
I opened the one sample project available for this board combo in CubeMX, uploaded it to the board without any problem.
Then I opened the project in CubeIDE, compiled without any problem, but uploading/running is returning these errors:
Error in final launch sequence:
Failed to execute MI command:
load C:\\TouchGFXProjects\\GFX01_Test01\\STM32CubeIDE\\Debug\\STM32G071_NUCLEO.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\GFX01_Test01\\STM32CubeIDE\\Debug\\STM32G071_NUCLEO.elf
Error message from debugger back end:
Load failed
Failed to execute MI command:
load C:\\TouchGFXProjects\\GFX01_Test01\\STM32CubeIDE\\Debug\\STM32G071_NUCLEO.elf
Error message from debugger back end:
Load failed
Load failed
And there is no external flashloader configured.
When I enable the external flashloader (S25FL032P_STM32G071B-NUCLEO, 0x90000000, SPI_FLASH, S25FL032P_STM32G071B-NUCLEO.stldr)
This is returned:
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (-2147155971) Unknown. Please check power and cabling to target.
2021-01-18 9:09 AM
Maybe it's related, but when I build the release in STM32CubeIDE, the .bin file is >2GB!
Is this because of this in the linker script:
SPI_FLASH (r) : ORIGIN = 0x90000000, LENGTH = 8M
2021-01-19 12:25 AM
A small update. I convert the generated .elf file to a .hex file (the .bin is way too big) : arm-none-eabi-objcopy -O ihex STM32G071_NUCLEO.elf STM32G071_NUCLEO.hex
Then I programmed the board by using "ST-Link Utility" and the external loader file (MX25L6433F_STM32G071B_NUCLEO.stldr) from the folder "en.X-CUBE-DISPLAY_1_0_0\Utilities\PC_Software\ExternalLoader".
And this is working fine, so the building in STM32CubeIDE is fine, only the uploading to the board is failing.
2021-01-19 1:45 AM
It's because .bin files do not contain notions of memory ranges, so it has to contain all the data from 0x0-0x90000000+8M. Disable bin file generation if you don't need it - You probably just want the .elf or .hex