2017-05-22 09:46 PM
Hi.
I'm using STemWin 5.28.
Today i was reading web page in seeger web. I find that the lastest EMWin version is V5.40 .U
nbelievable,I find the function
in the chapter '2-D Graphic Library' GUI_QR_Creat(), GUI_QR_Delete()....
Now ,Which version of STemWin support QR_Code ? HOW can i get the lastest version?
I'm using STM32f103vet6.
Best regards.
#qr_code #stemwin2017-05-30 05:02 AM
Hi
yongchao.zhao
,QR-Codes functionadded in the STemWinversion 5.
Today,
the
STemWin-library is based on version V5.28 for the last version of STM32CubeF1 V1.4.0.So,you can't use the
QR-Codes functions
since it is not available in the STemWin 5.28 with the last firmware package.Thanks
Imen
2017-05-31 08:51 PM
Thank you for your help. I hope ST updates the lib as quickly. Now i only use the libqrencode written by fukuchi.
Best regards!