2019-01-28 12:18 AM
Hello,
I would like to use a lot from the ST32L4R9I-DISCO Demo Code for my own application.
Are you planning to release the source code?
Thanks and best regards,
Christoph
Solved! Go to Solution.
2019-02-05 04:05 AM
2019-01-28 02:04 AM
Do you mean Disco or Nucleo or Eval. Only a Eval board is found on the website. Did you check
STM32Cube/Repository/STM32Cube_FW_L4_V1.13.0/Projects/STM32L4R9I-EVAL/Examples/?
2019-01-28 02:50 AM
Hi @Christoph,
I'm pretty sure the source code for the demo in question is not a part of the Cube firmware pack. I will check to see if i can make it available.
Best regards,
Martin
2019-01-28 02:57 AM
Hi @Martin KJELDSEN
I have checked all available Code but the TouchGFX demo for ST32L4R9I-DISCO was only available as binary :sad_but_relieved_face: .
Thanks, that would be very nice =) and I think also other developers would appreciate it.
Best regards,
Christoph
2019-02-01 09:46 AM
Yes, I would love to take a look at the source code to determine some of the features to implement as well.
2019-02-05 04:05 AM
2019-02-05 05:09 AM
Hi @Martin KJELDSEN
thanks a lot for providing the demo code =) , it will be very helpful for developing my application.
Best regards,
Christoph
2019-02-05 07:18 AM
Hi @Martin KJELDSEN ! Thanks a lot for procuring the source code for us! It'll be super helpful!