cancel
Showing results for 
Search instead for 
Did you mean: 

Slow fade and move effects when running from QSPI Flash

João Costa
Associate III

I'm using a STM32F7508-DK boar, so I need to run my code from QSPI flash. My application is running on target, but all the animations are slower than it should be. When running on simulator, everything runs perfect. Screen transitions without effects seems ok too! Attached ia video running a logo fade (time = 500ms). Did anyone have this problem too? Thanks a lot!

11 REPLIES 11

Good news! I was running build in debug mode. When running it on release mdoe, the code runs freely on my board! My fault, Thanks.

Okay, that's good news!! :)