cancel
Showing results for 
Search instead for 
Did you mean: 

sending a callback from a button inside a container (wheel item) to the view

nico23
Senior II

I have a scroll wheel languageSelectorWheel with several items. Every item is a container languageSelectorItem

On the container I have a toggle button. When I click any toggle button, I want to send a trigger on the view of the scroll wheel to execute a function.

nico23_1-1744798309967.png

 

On the toggle button I have added an interaction onClick via TouchGFX that emits the trigger languageChanged. The trigger is set on the languageSelectorItem container

nico23_0-1744798288466.png

On the view where the languageSelectorWheel is added, I have set the callback

void languageSettingsView::languageChanged()
 
Unfortunatly, it seems it is not called when i toggle the button (settings a breakpoint on the line that call 
emitLanguageChangedCallback(); in languageSelectorBase where void languageSelectorBase::buttonCallbackHandler(const touchgfx::AbstractButton& src) is defined enters)
 
My thought is that because the trigger is set on the container, it won't be passed to the view
1 ACCEPTED SOLUTION

Accepted Solutions
nico23
Senior II

Ok so I figure it out. I set a trigger on the container that returns its index

nico23_0-1744871336082.png

On the interactions I have added a button click that both call a function and executes the trigger

nico23_1-1744871388680.png

languageItem.hpp (container)

Here you must register the trigger

void setLanguageSelectedCallback(touchgfx::GenericCallback<const int16_t>& callback) { languageSelectedCallback = &callback; } protected: int16_t itemNumber; touchgfx::GenericCallback<const int16_t>* languageSelectedCallback;

languageItem.cpp (container)

here you execute the callback

void languageItem::buttonClicked() { // Call the callback when the button is clicked, passing the item number if (languageSelectedCallback && languageSelectedCallback->isValid()) { languageSelectedCallback->execute(itemNumber); } }

languageSettingsView.hpp

Here you register the callback from the container

protected: /* * Callback Declarations */ touchgfx::Callback<languageSettingsView, const int16_t> languageItemLanguageSelectedCallback; /* * Callback Handler Declarations */ void languageItemLanguageSelectedCallbackHandler(const int16_t itemIndex);

 

languageSettingsView.cpp (view)

Finally in the view you can initialize all the callback, one for each element of the wheel

languageSettingsView::languageSettingsView(): languageItemLanguageSelectedCallback(this, &languageSettingsView::languageItemLanguageSelectedCallbackHandler) { for (int i = 0; i < languageSelectorScrollListItems.getNumberOfDrawables(); i++) { languageSelectorScrollListItems[i].setLanguageSelectedCallback(languageItemLanguageSelectedCallback); } }

And then you can use the callback on the View to react according to the index

void languageSettingsView::languageItemLanguageSelectedCallbackHandler(const int16_t itemIndex) { }

Clearly on the View you need a function that set the itemNumber, something like

void languageSettingsView::languageSelectorScrollUpdateItem(languageItem& item, int16_t itemIndex) { item.setItemNumber(itemIndex); }

Where the setItemNumber function must be added to the container

View solution in original post

1 REPLY 1
nico23
Senior II

Ok so I figure it out. I set a trigger on the container that returns its index

nico23_0-1744871336082.png

On the interactions I have added a button click that both call a function and executes the trigger

nico23_1-1744871388680.png

languageItem.hpp (container)

Here you must register the trigger

void setLanguageSelectedCallback(touchgfx::GenericCallback<const int16_t>& callback) { languageSelectedCallback = &callback; } protected: int16_t itemNumber; touchgfx::GenericCallback<const int16_t>* languageSelectedCallback;

languageItem.cpp (container)

here you execute the callback

void languageItem::buttonClicked() { // Call the callback when the button is clicked, passing the item number if (languageSelectedCallback && languageSelectedCallback->isValid()) { languageSelectedCallback->execute(itemNumber); } }

languageSettingsView.hpp

Here you register the callback from the container

protected: /* * Callback Declarations */ touchgfx::Callback<languageSettingsView, const int16_t> languageItemLanguageSelectedCallback; /* * Callback Handler Declarations */ void languageItemLanguageSelectedCallbackHandler(const int16_t itemIndex);

 

languageSettingsView.cpp (view)

Finally in the view you can initialize all the callback, one for each element of the wheel

languageSettingsView::languageSettingsView(): languageItemLanguageSelectedCallback(this, &languageSettingsView::languageItemLanguageSelectedCallbackHandler) { for (int i = 0; i < languageSelectorScrollListItems.getNumberOfDrawables(); i++) { languageSelectorScrollListItems[i].setLanguageSelectedCallback(languageItemLanguageSelectedCallback); } }

And then you can use the callback on the View to react according to the index

void languageSettingsView::languageItemLanguageSelectedCallbackHandler(const int16_t itemIndex) { }

Clearly on the View you need a function that set the itemNumber, something like

void languageSettingsView::languageSelectorScrollUpdateItem(languageItem& item, int16_t itemIndex) { item.setItemNumber(itemIndex); }

Where the setItemNumber function must be added to the container