cancel
Showing results for 
Search instead for 
Did you mean: 

scrollWheel index incorrect, not responsive

FJB2069
Senior

I want to create a scrollWheel that has 3 preset options.  Option A, Option B,  and Option A&B

The issue I have is that I can never get itemIndex  = 1 in scrollWheelUpdateItem callback , only index 0 and 2.  Also, after I first change wheel, it takes a while to be able to change it again.

I tried to provide all the relevant code and touchgfx setup.  

Appreciate if you can tell me what is incorrect.

 

Here is my Container  (MenuItem):

FJB2069_1-1737391403340.png

Here is how I set up my text:

FJB2069_0-1737391266784.png

scrollWheel:

FJB2069_2-1737391503713.png

 

Here is Container MenuItem.cpp:

#include <gui/containers/MenuItem.hpp>
#include <texts/TextKeysAndLanguages.hpp>
#include <BitmapDatabase.hpp>


MenuItem::MenuItem()
{

}

void MenuItem::initialize()
{
    MenuItemBase::initialize();
}

void MenuItem::setWheelElements(int item)
{
	switch (item)
	{
	case 0:
		text.invalidate();
		text.setTypedText(TypedText(T_S1));
		break;
	case 1:
		text.invalidate();
			text.setTypedText(TypedText(T_S2));
			break;
	case 2:
		text.invalidate();
			text.setTypedText(TypedText(T_S3));
			break;

	}

}

MenuItem.hpp:

#ifndef MENUITEM_HPP
#define MENUITEM_HPP

#include <gui_generated/containers/MenuItemBase.hpp>

class MenuItem : public MenuItemBase
{
public:
    MenuItem();
    virtual ~MenuItem() {}

    virtual void initialize();
    void setWheelElements(int item);
protected:
};

#endif // MENUITEM_HPP

Buttons1MenuView.cpp

#include <gui/buttons1menu_screen/Buttons1MenuView.hpp>
#include <gui_generated/common/FrontendApplicationBase.hpp>
#include "config_file.h"
#include "math.h"


Buttons1MenuView::Buttons1MenuView()
{

}

void Buttons1MenuView::setupScreen()
{
    Buttons1MenuViewBase::setupScreen();

    
}

void Buttons1MenuView::tearDownScreen()
{
    Buttons1MenuViewBase::tearDownScreen();
}


void Buttons1MenuView::scrollWheelUpdateItem(MenuItem& item, int16_t itemIndex)
   {
	scrollWheel.invalidate();  //NOT SURE IF NEEDED
   	item.setWheelElements(itemIndex);

   }

Buttons1MenuView.hpp

#ifndef BUTTONS1MENUVIEW_HPP
#define BUTTONS1MENUVIEW_HPP

#include <gui_generated/buttons1menu_screen/Buttons1MenuViewBase.hpp>
#include <gui/buttons1menu_screen/Buttons1MenuPresenter.hpp>

class Buttons1MenuView : public Buttons1MenuViewBase
{
public:
    Buttons1MenuView();
    virtual ~Buttons1MenuView() {}
    virtual void setupScreen();
    virtual void tearDownScreen();
   
    virtual void scrollWheelUpdateItem(MenuItem& item, int16_t itemIndex);





protected:
};

#endif // BUTTONS1MENUVIEW_HPP

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions

I missed that, thank you!

View solution in original post

8 REPLIES 8
FJB2069
Senior

I increased the size of the scrollWheel window (still making it only show one item) it responds much better and I do now get valid itemIndex, accept the index number does agree to what I thought it should be.

FJB2069_1-1737395078839.png

In other words,  I assume Option A should have index 0,  Option B index 1 and Option AB index 2,

but I get Option A index 1, Option B index 2 and Option AB index 0

Anyone know why the indexes as not as expected?

 

GaetanGodart
ST Employee

Hello @FJB2069 ,

 

Getting the "right" index when using a scrollWheel is tricky.
This is because it is not meant to be accessed. Instead, the scrollWheel should be used as a menu selector to navigate through your application or to select various options.
Therefore, you should only use the 2 callbacks provided setitempressedcallback and setitemselectedcallback .

So in a way I am avoiding your question because this is not how you should use the scrollWheel and I invite you to not use the index but only the 2 callbacks if you can.
If you really want to use the index of the elements, you should use the scrollList.

 

I hope this helps.

 

Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

I changed from a scrollWheel to a scrollList.  I get exact same results.

 

1) How might I implement setitemselectedcallback in my existing code?  

I tried below, but will not trigger?

2) Also,  I need to initialize the scrollList.  How can I do this in Buttons1MenuView::setupScreen()?

 

Buttons1MenuView.hpp

 

#ifndef BUTTONS1MENUVIEW_HPP
#define BUTTONS1MENUVIEW_HPP

#include <gui_generated/buttons1menu_screen/Buttons1MenuViewBase.hpp>
#include <gui/buttons1menu_screen/Buttons1MenuPresenter.hpp>

class Buttons1MenuView : public Buttons1MenuViewBase
{
public:
    Buttons1MenuView();
    virtual ~Buttons1MenuView() {}
    virtual void setupScreen();
    virtual void tearDownScreen();
    virtual void buttonRGOPressed();
//    virtual void button2H1BPressed();
//    virtual void button2H2BPressed();
    virtual void scrollListUpdateItem(MenuItem& item, int16_t itemIndex);
    virtual void scrollListItemSelectedCallbackHandler(const touchgfx::ScrollList&, int itemIndex);




    void saveCurrentScreenIndex(int screenIndex)
               {
              	 presenter->saveCurrentScreenIndex(screenIndex);
               }

               int getCurrentScreenIndex()
               {
              	 return presenter->getCurrentScreenIndex();

               }

protected:
               touchgfx::Callback<Buttons1MenuView, const touchgfx::ScrollList&, int> itemSelectedCallback;
};

#endif // BUTTONS1MENUVIEW_HPP

 

Buttons1MenuView.cpp

 

#include <gui/buttons1menu_screen/Buttons1MenuView.hpp>
#include <gui_generated/common/FrontendApplicationBase.hpp>
#include "config_file.h"
#include "math.h"

static int8_t index_trig;
static int position;


Buttons1MenuView::Buttons1MenuView() : itemSelectedCallback(this, &Buttons1MenuView::scrollListItemSelectedCallbackHandler)
{
    // Initialization code for ScrollList, if needed
	
}



void Buttons1MenuView::setupScreen()
{
    Buttons1MenuViewBase::setupScreen();

    saveCurrentScreenIndex(8);






}

void Buttons1MenuView::tearDownScreen()
{
    Buttons1MenuViewBase::tearDownScreen();
}


void Buttons1MenuView::buttonRGOPressed()
  {
      // Override and implement this function in Buttons1Menu

		 if(textButtonRGO.isVisible())
		 {
			 //turn off
			 CONFIG.RGOMode[CONFIG.mode]=0;
			 textButtonRGO.setVisible(0);
		 }
		 else
		 {
			 CONFIG.RGOMode[CONFIG.mode]=1;
						 textButtonRGO.setVisible(1);
		 }
		 textButtonRGO.invalidate();
  }


void Buttons1MenuView::scrollListUpdateItem(MenuItem& item, int16_t itemIndex)
   {


	if(itemIndex==0)
		index_trig = itemIndex;
	else if(itemIndex==1)
		index_trig = itemIndex;
	else if(itemIndex==2)
		index_trig = itemIndex;

		item.setWheelElements(itemIndex);

		scrollList.invalidate();
		index_trig = itemIndex;


   }


void Buttons1MenuView::scrollListItemSelectedCallbackHandler(const touchgfx::ScrollList&, int itemIndex)
{
	// Handle item selection here
	position = itemIndex;
	// Example: Update a text area with the selected item
	// Unicode::snprintf(selectedItemTextBuffer, TEXT_BUFFER_SIZE, "Selected: %d", itemIndex);
	// selectedItemText.invalidate();
}

 

 

 

Hello @FJB2069 ,

I'm not sure about the issue you're having. I've tried on my side to make an application similar to what you want to achieve (from what I understood). It works fine on my side. I'm sharing it here. Please let me know if this was what you wanted to achieve.

Osman SOYKURT
ST Software Developer | TouchGFX

Thank you for your help!

 

 I see that the <value>  (0,1,2) is being updated correctly from ScrollWheel.  I am not understanding how the ScrollWheel is sending the S1,S2,S3 index to the <value>?  How is the Scrollwheel linked to textArea2?

Hello @FJB2069 ,

 

In Screen1View.cpp it is this function that updates the textArea's wildcard:

void Screen1View::scrollWheelAnimateToHandler(int16_t itemSelected)
{
    Unicode::snprintf(textArea2Buffer, 3, "%d", itemSelected);
    textArea2.invalidate();
}

 

 Regards,

Gaetan Godart
Software engineer at ST (TouchGFX)

I missed that, thank you!

My pleasure! :smiling_face_with_smiling_eyes:

Gaetan Godart
Software engineer at ST (TouchGFX)