cancel
Showing results for 
Search instead for 
Did you mean: 

" ​STM32F429I Discovery Button sample demo " example error occurs

mSH.1
Associate III

hello

" ​STM32F429I Discovery Button sample demo " during the examples of TouchGFX.

0693W00000Nrg6xQAB.png

An error occurs in the project created in TouchGFX.

The error contents are as follows.

0693W00000Nrg72QAB.png

It is an error that the #include "stm32f429i_discovery.h" file cannot be found, but the folder does not exist in Drivers.

0693W00000Nrg7CQAR.png

Add to

If you download it to the board directly from touchGFX, it works normally.

However, when I run the project in STMCubeIDE and build it, the above error occurs.

What should I do?

thank.​

7 REPLIES 7
mSH.1
Associate III

Add to

If you download it to the board directly from touchGFX, it works normally.

However, when I run the project in STMCubeIDE and build it, the above error occurs.

Osman SOYKURT
ST Employee

Hello mSH.1,

Thank you very much for reporting this issue. We're currently working on it. I'll keep you updated when we have a patch for that.

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX

Hello Oskt

Thanks for checking.

ETAN1
Associate

Are there any updates on the example? @Osman SOYKURT​ 

Hello ETAN,

We're on it. We might delete this demo which run on the STM32F412-DISCO but we planned to make an other one using an other board. Do you mind it ?

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX

Hello @Osman SOYKURT No, I don’t mind at all. But I'd like to see a board-specific demo working on the STM32F429I-DISC1 board. Because I'm a bit confused about what's the proper way to interacting with the hardware.Thank you!

Ok, no worries, it will be the same demo (button example) but it might work on another board though.

If you need tutorials about how to interact with the hardware, we have some videos on on Youtube channel that explains step by step how to make it. I invite you to have a look at it ;)

https://youtu.be/4-fyx4e96jk

https://youtu.be/ufvJ5bcesL8

https://youtu.be/QgEDSjvGAlk

/Osman

Osman SOYKURT
ST Software Developer | TouchGFX