[Question] How to configure cubeMX for touchgfx and supplemental touchscreen MB1315A on a STM32L4R9I-EVAL?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-05-28 11:23 AM
Hi,
I'm absolutely failing to deploy a successful touchGFX UI on the MB1315A . I can get a touchgfx example deployed on the onboard 390x390 LCD. However, in order to deploy to alternative screens, the documentation says to go through CubeMX.
And so I went through cube MX. I setup the touchGFX generator, freeRTOS, and LTDC, and all other HW components, but it still fails.
I was following this documentation to try and deploy the touchGFX application.
- https://support.touchgfx.com/docs/4.15/development/touchgfx-hal-development/touchgfx-generator
- https://support.touchgfx.com/docs/4.15/development/touchgfx-hal-development/scenarios/scenarios-ltdc-parallel-rgb
However, the touchGFX generator throws an error/warning surrounding the parameter settings of the LTCD.
- Documentation states nothing about what to se the synchronization settings to. Only the layer settings -> start/stop values.
- So I filled in the synchro settings: https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Projects/STM32L4R9I-EVAL/Examples/LTDC/LTDC_Display_1Layer
- Current error states: Width/height values must equal LTDC Window width/height/
I have additional questions surrounding the configuration of the LTDC. Based on the documentation for setting up the MB1315A, I can't find a setting about the MFX_GPIO_11/12.
- I don't know what to set these values to CubeMX!
- PA_11/12 currently set to GPIO_EXTI11/12
- https://www.st.com/resource/en/user_manual/dm00407907-evaluation-board-with-stm32l4r9ai-mcu-stmicroelectronics.pdf
- See page 45 for LTCD. See page 43 for MFX mapping
I also have no idea what to set the RCC, SYS, TSC, and I2C2 values to. I have attached my current .ioc file so one may examine, laugh, and help =)
Overall, I need a successful .ioc file which can deploy on STM32L4R9I-EVAL and the supplemental touchscreen MB1315A.
Needs
- FreeRTOS
- TouchGFX
If there is an example application that meets all of these needs, I would be extremely grateful.
Much appreciated
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-01 4:08 AM
Hi,
I can maybe point out that the STM32H7B3dk board uses the same MB1315A display, so you could have a look at the application template for that board available in TouchGFX Designer and use it as source of inspiration for your settings + touch controller configuration.
​
If you started from the application template for the STM32L4R9-eval from TouchGFX Designer, you should pay attention to remove the GFXMMU settings as they are meant to be used for a round display configuration.
For the error states "Width/Height values must equal LTDC Window width/height", well you can fix it by setting them to the same thing :grinning_face_with_sweat:. It should be under the "LTDC" settings, in the "Layer Settings" tab. Make sure the framebuffer and the windows position settings are the same for the height and width.
​
/Romain
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-10 9:24 AM
Hey Romain,
Thanks for your feedback.
I was able to resolve all of the dependency issues between the LTDC, DMA, and FreeRTOS. But I still am not able to successfully run LTDC graphical renderings on the touchscreen.
I greatly simplified the program and took it back to basics. I dropped: touchGFX, freeRTOS, DMA2D, everything but the LTDC controller. But the LTDC controller is still NOT working when generated from a .ioc file and working from the datasheet. Currently, the screen initializes to completely white despite having a framebuffer of a picture.
I am able to compile and run a LTDC example from the STMicro examples folder for the L4R9.
- https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Projects/STM32L4R9I-EVAL/Examples/LTDC/LTDC_Display_1Layer
- Why do none of the examples provide .ioc files for CubeMX configuration? :(
When it comes to my .ioc I know that certain hardware settings are correct because I have transplanted the init code from mine to the example, and the example still works. However, others must not be!
- LTDC init code
- Passes
- RCC and clocks
- Passes
- I2C2 - Trigger backlight
- Passes
I am very concerned about the GPIO init process generated for my main.c. The example provides no code information about their GPIO.
- Mostly concerned with the i2c expander GPIO that might not be triggering correctly (Pg. 45 as stated earlier):
- MFX_GPIOI11
- MFX_GPIOI12
- I don't know how to find out their gpio init process and translate it into .ioc configuration -> my main.c
I have attached my entire project. But I would be eternally thankful if someone could peek at the .ioc and main file and tell me what I am doing wrong.
I have also used the following resources to try and learn more already:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-10 9:28 AM