cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with creating .bin files

cb.7
Associate III

Hello,

I am developing an application with:

  • lcd with ILI9341
  • STM32F411RET6
  • SPI external flash memory model SST26VF032B

I have already created the .stldr file for this memory and it works fine.

I edited the STM32F411RETX_FLASH.ld file to add the external flash.

I create the project from CubeMX, enable TouchGFX, create a test screen and do "Generate Code".

Why are the .bin files of the bitmaps and fonts not created to put in the external flash?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Maybe there are problems with my custom external loader.

Is there an example code for external loader for SPI?