2020-07-08 11:40 AM
My original problem is when I try to see a GUI example running, when I hit on "Run Simulator" the operation fails and in the detailed log appears the following message:
"Generate Assets
make -f simulator/gcc/Makefile assets -j8
0 [main] us 0 init_cheap: VirtualAlloc pointer is null, Win32 error 487
AllocationBase 0xC90000, BaseAddress 0xDC0000, RegionSize 0xCD000, State 0x2000
C:\TouchGFX\4.13.0\env\MinGW\msys\1.0\bin\sh.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0
make: *** [assets] Error 1
simulator/gcc/Makefile:32: recipe for target 'assets' failed
Failed
Failed"
I tried with different application templates and UI templates but the error is the same.
I saw on other thread a possible solution:
But it did not work for me to rebase msys-1.0.dll, here are the details:
I executed the same command as recommended but it did not work:
"editbin /rebase:base=0x50000000 msys-1.0.dll"
"msys-1.0.dll : fatal error LNK1342: failed to save a backup copy of the binary file to be edited"
Then I tried to execute it with msys-1.0.dll file which is contained in TouchGFX at C:\TouchGFX\4.13.0\env\MinGW\msys\1.0\bin\msys-1.0.dll but it seems nothing happened because the problem remained.
I executed above commands from the Visual Studio command prompt as stated here:
https://docs.microsoft.com/en-us/cpp/build/reference/editbin-reference?view=vs-2019
Please help
2020-07-09 01:30 AM
Hi. Do you have multiple msys.dlls in your path? From other tools.
2020-07-09 01:53 AM
I don't know for sure, I only have these in my path...
I formatted my computer a few days ago, I am recently installing everything again, so I don't have that many applications. Before formatting I had run TouchGFX and it worked properly.