2018-12-24 10:24 PM
Hi
Another problem with Animated Image example at win 10
log file is enclosed ,
I could run the same example at win 7
Can anybody help
2019-01-02 06:34 AM
I just tried installing a windows 10 virtual machine and running the designer with Turkish regional/language settings. I could compile and run applications, so it's not that.
Could you try reinstalling the designer to some other location just to rule out any issues with the installation?
2019-01-02 07:09 AM
@Community member , you can use the free service from WeTransfer:
to share your project.
2019-01-02 10:14 PM
Good Morning
Which email address I should use at wetrasfer.com to share project folder
2019-01-03 04:48 AM
@Community member - no, once the upload is ready, the Wetransfer website will generate a new URL to share. This upload will be active for 7 days.