cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with Animated Image example at win 10

AKINI
Associate III

Hi

Another problem with Animated Image example at win 10

log file is enclosed , 

I could run the same example at win 7 

Can anybody help

23 REPLIES 23
Martin KJELDSEN
Chief III

Hi!

I'm seeing a few different errors in the logfile. Before getting into those - What happens with your application on Windows 10?

Thanks!

Hi Martin Thank you for your answer

error window enclosed

Thank you for the update!

And you're using TouchGFX 4.10.0 ?

AKINI
Associate III

Yes but I tried 4.9.3 also

Martin KJELDSEN
Chief III

<duplicate post>

Thanks!

Did you create the application itself on a windows 7 machine and are now trying to run it on Win10?

AKINI
Associate III

I have win 7 at my home

I tried example and new project without any problem at win 7

At work I have another pc with win 10 .I couldnt simulate or compile anything here

I just tried the AnimatedImage example with TouchGFX 4.10.0 on my Windows 10 machine - No problems here.

Which language is your Windows 10 at work? And just to be 100% sure - This is your procedure?

1) Start designer

2) Create new application with Simulator Application Template and Animated Image UI Template

3) "Run Simulator" gives you the error in your log

Thanks!

Best regards

Martin

AKINI
Associate III

Hi

I tried again as you said

Error during code generation

and same error window