2024-05-16 10:00 AM
Hello,
I am new at the STM32 World.
I started to buy a nucleo-f767zi and it worked fine.
I was not able to get the debug Console running. Like other too.
Because of that I bought the extension Board x-nucleo-GFX02zi which should be working fine with the F767ZI.
Now I tried with CubeMX to installed the Hello World Example provided.
But now I get the Message that these Packets is not Support with CubeMX 6.11. It should be support by Version 6.7 until 6.8.2.
I tested 6.8.2 and 6.8 but without any changes. It seams like the SPI does not fit together. Always I got no solution found.
Does the GFX02zi can be used with the F767ZI? Or do I have to everything new.
I am going a bit crazy.
Is there anyway a working step by Step intruduction for Add a Display to a STM32.
Thanks for any help
best regards
Carsten
Solved! Go to Solution.
2024-05-23 06:51 AM
Thanks. exactly.
But the test and prototype no a GUI and PINs.
Because of that, I bought a simple LCD SPI Display which is very good documented and Howto`s are available.
I hope this way I can achieve success more quickly.
Thanks
Carsten
2024-05-23 07:18 AM
Sure, not problem. We provide our board + display setup just for easy of use.
Just out of curiosity, may I know what display you went for?
2024-05-23 07:21 AM
I bought a simply ILI9341 SPI one.
I saw enough documentation and explanations howto.
I am looking foward to get it running next week.
carsten
2024-05-23 07:35 AM
Oh ok.
Yes, a lot of people use it so there is a lot of documentation about it but it is also all over the place, it is a mess. :grinning_face_with_sweat:
I personally think we should make a TBS or 2 for this display and maybe some more for other ILI9xxx.
2024-05-23 07:46 AM
would be helpful.
If you like I can tell you my result, next week
2024-05-23 07:48 AM
Sure, that would help us if we end up doing a TBS for it (and that would also help me convince the product owner)!