2019-09-11 1:24 AM
I can't no longer import TouchGFX GUI, every time i try i get :" Import failed, UI is not compatible, but it is, same display size, even same board keep saying that. also ruin my project because when he try to import the GUI, he delete some elements (mostly images).
then if i try again to import same GUI, he gives me Unexpected error has happened
italian part says :" process can't access to (path) because it's in use by another process... but nothing is using that, i have no other programs running.
i also attached the log file, hope someone can help me figure this out
Thanks
Stefano
2019-09-23 1:33 AM
Yes, the import-feature does not support upgrading a project in the process because this might not be the intention for the imported project. But the error message could be better!
So, in a nutshell, if your project is 4.10.0 and the project being imported from is, let's say 4.23.0, you can't import the gui because it is impossible to downgrade 4.23 -> 4.10. But, if your projects are the same version the import will go well.
Which version are you trying to import from?
/Martin
2019-09-23 1:37 AM
from 4.10 to 4.10... (now give me link to the secret 4.23 please XD)
2019-09-23 1:44 AM
Haha, 23 was an arbitrary number.
4.10 to 4.10 - This shouldn't cause you any issues. Are you able to send these projects to me?
/Martin
2019-09-23 1:57 AM
I'm sending you the project (just one, because the other is a brand new f746g-disco project)
thanks