cancel
Showing results for 
Search instead for 
Did you mean: 

Configure stm32h747i-disco touch screen to make a graphic interface.

slimani
Associate II

I am a student in embedded systems. I have a final project with the stm32h747i-disco card. I want to configure the touch screen to make a graphic interface.

26 REPLIES 26
mƎALLEm
ST Employee

Hello @slimani and welcome to the ST community,

Please use TouchGFX designer tool to create a ready-to-use graphic project based on that board. The hardware will be configured automatically: LCD, Frame buffer, TouchScreen, memories, etc ..

As shown in this screenshot, find your board and click on create button:

mALLEm_0-1743781022473.png

Hope that answers your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I do this and upload the project but the stm32h747i-disco screen does not work

What do you mean by " does not work" you need to give more details what you did exactly and what are the symptoms of the issue.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
slimani
Associate II

I am making a project on touchgfx and I upload this project to the card but the card screen does not work remains black please help me 

 

slimani
Associate II

I also activate the timer but the screen always remains black and does not light up.

Hello,

You are using a dual core product and there are two projects related to both cores CM4 and CM7. Make sure to upload the two binaries of both cores:

mALLEm_0-1743865758321.png

No relation with activating a timer with the display.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

I do all that but nothing changes the screen remains black does not turn on can you give me the steps to test the screen

Download this STM32H747I-DISCO compiled demo binary (use STM32CubeProgrammer). If the blackscreen still there, I assume your board is broken. 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
slimani
Associate II

I download it how do I upload it to stm32