2021-10-13 10:00 PM
Is there a good way for multiple people to develop their screens and integrate them into the same TouchGFX project?
Solved! Go to Solution.
2021-10-14 04:56 AM
Hi,
At the moment no but we should release TouchGFX 4.18 in one or two weeks which will have "multiple engineer support" as we call it where you can have multiple people working on a same TouchGFX project with git. They should however work on their own screens to avoid issues when merging.
/Romain
2021-10-14 04:56 AM
Hi,
At the moment no but we should release TouchGFX 4.18 in one or two weeks which will have "multiple engineer support" as we call it where you can have multiple people working on a same TouchGFX project with git. They should however work on their own screens to avoid issues when merging.
/Romain
2021-10-14 05:11 AM
Thank you very much.