Missing parameter in LCD_LL_DrawBitmap8bpp
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-22 4:13 AM
According to the emWin manual LCD_SetDevFunc can be used to set additional and / or user defined functions of the display driver.
Examples from STM32CubeF4 are using the function within LCDConf_xxxx.c to set a low layer drawing function for 8bpp bitmaps like
LCD_SetDevFunc(i, LCD_DEVFUNC_DRAWBMP_8BPP, (void(*)(void))LCD_LL_DrawBitmap8bpp);
to use DMA2D for the data transfer. However the emwin manual says:
LCD_DEVFUNC_DRAWBMP_8BPP
Can be used to set up a function which draws 8bpp palette based bitmaps. This can
make sense if for example a BitBLT engine is available to do the job.The function pointed bypDriverFunc
should be of the following type:
void DrawBMP8(int LayerIndex,
int x, int y, U8 const * p, int xSize, int ySize,int BytesPerLine, const LCD_PIXELINDEX * pTrans);whereas the passed function pointer in LCDConf_xxxx has the following signature:
static void LCD_LL_DrawBitmap8bpp(int LayerIndex, int x, int y, U8 const * p, int xSize, int ySize, int BytesPerLine)
So the last parameter pTrans is missing. Don't know if this is a problem, but it should be fixed because emWin is passing pTrans anyway.
#stemwin- Labels:
-
STemWin
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-23 7:52 AM
Hello,
I raised your issue internally to the appropriate team.
Thank you for your contribution.
Best Regards
Imen
Thanks
Imen