2020-01-05 11:46 PM
Hi @Martin KJELDSEN
First of all I wish you a happy new year. I hope you started well in the new year
I've updated TouchGFX from 4.12.3 to 4.13.0 and I have the following issues:
The TouchGFX Generator changes the slashes from \ to / in the paths (e.g. include paths) of the ewp file (IAR)
The bug with the fonts is sill not solved -> see this thread
/Marco
Solved! Go to Solution.
2020-03-27 05:36 AM
Hi @Martin KJELDSEN
Thanks for fixing the bug with the font converter. I've found it on your new TouchGFX Documentation, which looks good.
/Marco
2020-01-06 01:20 AM
Hi Marco,
I did, thank you. Hope you did too!
I don't remember which version i sent you, but the one you have is most likely a release candidate:
Can you be more specific about the issue with slashes? I need concrete examples posted here.
I wouldn't rule out the "bug" you're mentioning being fixed in the final release either.
/Martin
2020-01-06 01:39 AM
You did not send me a version. It is possible to download the current version through CubeMX -> see another thread
The new TouchGFX generator changes the slashes of the include paths (see diffs of *.ewp file)
... and also paths of the files itself
/Marco
2020-01-06 02:02 AM
I've just verified that you can actually get it through CubeMX 5.4.
It's actually the post-generate step through the designer that does this. Just commit it and let the post-generate script update it from now on?
/Martin
2020-01-06 03:01 AM
So the bug with the fonts is not fixed yet?
Is it not possible to change the post-generate script? We have had some problems in the past in a different project, when we used different types of slashes in the include path.
Based on this, we have to go back to version 4.12.3
2020-01-06 03:51 AM
Please create a 4.13.0 project for me that exhibits the issue with additional generated glyphs for this particular font. I'm not ready to blame the fontconverter or designer just yet : )
/Martin
2020-01-06 09:47 PM
2020-01-21 11:15 PM
Hi @Martin KJELDSEN
Do you have any update about the fontissue? I added a project 2 weeks ago. Had you time to try it out? Can you confirm that there is an issue?
Thanks
/Marco
2020-03-12 04:55 AM
Hi @Martin KJELDSEN
Do you have any update about this bug? I would appreciate an answer.
Thanks
/Marco
2020-03-27 05:36 AM
Hi @Martin KJELDSEN
Thanks for fixing the bug with the font converter. I've found it on your new TouchGFX Documentation, which looks good.
/Marco