2019-06-18 11:32 AM
I am working on an application that will need to be able to allow the user configure the color scheme of the screen. That is, the color of various images will need to be changeable. Is there a way do this with the TouchGFX libraries? What I would like is to have a basic image and be able to paint it using the libraries. I did not see any examples of this provided.
I would prefer to not have multiple images in the assets, each of a different color because the number of different colors this application will require.
Or would this require drawing the image in code with the abstract shape class and then paint it?
2019-06-18 01:31 PM
Hi Scott,
I'm not entirely sure what you mean by changing the color of images. Images can be complex.
If you insist, you can get the image data from any image and "go to town" on the data, changing it however you want. If you have static Bitmaps that reside in QSPI then that data is static, but you could create a DynamicBitmap and copy the static data to this new images buffer and modify it there.
Let me know. I think i'm missing a few pieces of the puzzle here.
/Martin
2019-06-18 01:38 PM
Martin,
Thanks for the quick reply. Sorry for my brief description.
In this case, the images would not necessarily be complex. It is possible that maybe they would be grey-scale and then "paint" or "tint" them as the user selects color schemes. The DynamicBitmap sounds promising but I am unfamiliar with it. I will look into it. Is there a tutorial describing/discussing it's functionality?
2019-06-18 02:16 PM
Hi Scott,
Okay. Then, it could be a solution to have one "template" as static data in qspi and then take the pixel data and modify that into dynamic bitmaps. There's no good documentation for this. Documentation is a mess right now to be honest and we're trying to figure out a strategy - Usage scenarios are become much more complex.
I've attached the dynamic bitmap example from 4.8.0. Give it a look - Maybe you can upgrade it to 4.10.0.
/Martin
2019-06-18 02:20 PM
Thanks Martin, I will take a look at it.
2019-07-10 08:42 AM
Martin,
I am just getting back to trying this. I looked over the example you provided and it uses a BMPFileLoader.
And when I look at this article:
https://touchgfx.zendesk.com/hc/en-us/articles/207460605-Dynamic-Bitmaps-Load-images-at-runtime
It refers to BMPFileLoader, but I cannot find it in the latest version of TouchGFX. Is it no longer supported?
I also found this discussion concerning it:
https://community.st.com/s/question/0D50X0000AYqpM7/where-is-bmpfileloader
Are we to write our own loader for this since it is not in TouchGFX 4.10.0 ?
Basically, what I want to do is load images that are part of the designer into a dynamic bitmap and manipulate it, which is turning into a larger task than I had anticipated.
2019-07-11 12:17 AM
Hi @scottSD,
The BMPFileLoader is not a framework construct which is why it's not in any release. You'll have to get it from that example i posted just above. The same goes for PNGFileLoaders, and whatever else you want to decode.
/MArtin
2019-07-11 08:47 AM
Thanks Martin. I didn't realize I needed to copy the files into my project.
I ended up doing something else that appears to work for me.
When a PNG image is dropped into the Designer, it becomes part of the BitmapDatabase and given an ID (in BitmapDatabase.hpp). Is the image now available to be cached? It appears so, because I was able to manually copy the source bitmap into the dynamic bitmap i created. I cached the source bitmap and read the address using cacheGetAddress(), then manually copied the source bitmap into the dynamic bitmap.
For some reason the function cacheReplaceBitmap() is returning false when I try using it to replace the contents of the dynamic bitmap with the source bitmap. The bitmaps are the same size, so not sure why it's returning false.
2019-07-11 11:18 PM
Hi Scott, don't be sorry! I guess it must not be very clear, but what we intended with the framework was to provide only the necessary constructs, anything else is provided as examples - For instance PNG and Bitmap decoders because they fall a bit outside, conceptually.
Can you debug the code and check where and why it's returning false?
/Martin
2019-07-11 11:25 PM
Maybe it's something to do with your cache size. Did you allocate a large enough buffer? The examples usually have to be modified a bit to suit your needs.
/Martin