cancel
Showing results for 
Search instead for 
Did you mean: 

Is mirroring the output image possible using the LTDC or DMA2D on STM32F746 ?

JStoe
Associate II

Hi,

We are a team of developers working on an electronic back mirror application (for cars and / or bicycles). We would like to create a functional demonstrator using a stm32F746-Disco board which we have on hand.

Since the image has to be mirrored we hoped that we could program the DMA engines of the LTDC or the DMA2D unit accordingly rathe rthan mirroring in SW ?

Best Regards,

Jan Stöfer

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
MM..1
Chief III

Hi

best choice is mirror on LCD driver or camera. Search control register to it, but this mirror full display

waclawek.jan
Super User

There's no hardware on the STM32s which can do this operation. As MM..1 said, choose a camera or LCD which support mirroring (i.e. changing scan order).

Although this won't help you directly, please consider voting for

https://community.st.com/s/ideazone#0873W000000PAuxQAG .

JW

JStoe
Associate II

Hi MM1, JW,

checked the datasheet of my camera. Looks like it probably can change scan order.

So I will go that way.

Thanks for your answers, which helped.

Jan