2021-01-27 10:15 PM
I have developed a custom keyboard in TouchGFX and it is working fine, but now i would need to change the alpha property of some keys, and also press the keys, all from the code. In order to press a button widget from code i do the following:
x=button->getX();
y=button->getY();
x+=5;
y+=5;
evnt = ClickEvent::PRESSED;
ClickEvent click1(evnt, x, y);
button->handleClickEvent(click1);
button-> invalidate();
evnt = ClickEvent::RELEASED;
ClickEvent click2(evnt, x, y);
button->handleClickEvent(click2);
button-> invalidate();
In the case of the keyboard i have tried to do something similar with the method "virtual void handleClickEvent(const ClickEvent& evt);" of the keyboard class, but anything happened. I would really appreciate any help. Thanks in advance.
2021-02-18 6:26 AM
Hi,
Were you able to fix your issue ? If not could you provide more context to your code?
Would it be possible to share your custom keyboard ? It may greatly help other users.
/Romain
2021-02-22 10:48 PM
Hi,
In the end i was not able to use it in that way, i had no time so i did my own keyboard with buttons. Besides, tha RAM used with the keyboard widget was huge, so i prefer this option.. Anyway, just in case it could be useful for someone i attach the files of the keyboard widget. I can not attach the whole project so i just upload the keyboard files.
2021-02-23 12:10 AM
The keyboard widget is quite old and needs some update/redesign (planned if I remember correctly). So thank you for sharing yours.
/Romain