cancel
Showing results for 
Search instead for 
Did you mean: 

Import touchgfx project to STM32F2

C.East2
Associate III

Hi there. I have a custom development board which uses a STM32F207ZG. The board uses an ILI9341 display driver and used uGUI for the UI previously. I understand that Touchgfx does not support an STM32F2 MCU, but is there any way to import the UI in anyway?

4 REPLIES 4
MM..1
Chief III

Problem isnt UI , but library. TouchGFX prebuild is Cortex M0 M33 M4 M7

But ST web say M3 too, then maybe somebody reply you info how...

It's a shame there isn't the option. Like you say, it's stated that the GUI runs on the M3.

Hi,

It used to support Cortex M3 but has been removed since there are no graphic oriented discovery kit made by STmicroelectronics. I have transfered this post to the marketing team as this is not the first time people are asking for it, so that they can maybe push for it.

/Romain

Thanks Romain, I want to take every step possible before having to bite the bullet and upgrade the hardware to an F429.