cancel
Showing results for 
Search instead for 
Did you mean: 

I want to know if it is possible to implement the attached gif image function with the "Progress" function.

mSH.1
Associate III

hello

I want to know if it is possible to implement the attached gif image function with the "Progress" function.

Is it possible to implement with gradient progress?

Or can you show me how to make a gradient image in advance with Image Progress?

0693W00000SvLfkQAF.jpg

Below is a Progress that repeats continuously to one side, but it cannot be implemented as a function provided as a Widget.

Is it possible?

0693W00000SvLfzQAF.gifthank.​

1 REPLY 1
wired
Senior III

I'll venture a guess and say probably not natively with the Designer's progress function, but you could make a custom 'progress' container with the gray bar image and the sliding bar image and execute a continuous move animation for the sliding bar. And your animation is really more of a busy indicator than a progress bar, isn't it? I am doing something similar to indicate an 'emptying' operation.

If you want to get really fancy and have the rounded ends, you will need a transparent mask the same size as the gray bar on top of the sliding bar.