2018-12-13 4:28 PM
Hi.
I will contact you with an unknown error.
When this error message is displayed, the run simulator, run tag, generater code, etc. can not be executed.
I noticed that some of the code in the 'generated' folder should be missing.
Please tell me how to fix it.
Below is an error message.
2018-12-14 4:52 AM
Hi,
Which version of windows are you using? Also, this issue can be related to low disk space preventing virtual allocation to function correctly. Could you check that?
Thanks!
2018-12-16 4:12 PM
why i can't delete this reply ㅠㅜ
Your administrator has disabled feed post and comment deletions.
2018-12-18 4:06 PM
Thank for your reply.
I use window7 professional.
Hard disk capacity remains 21gb.
2019-01-02 4:43 PM
I solved this problem partly by changing the base address of msys-1.0.dll.
The code in ac6 is still not created properly.
I am trying to fix the error code.