cancel
Showing results for 
Search instead for 
Did you mean: 

I want to change the resolution

Ebun.1
Senior

Hello

​

In the case of F746-DISCO, the resolution is 480 × 272,

For example, how to customize when connecting 800x600 LCD?

​

Thank you.​

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
HP
Senior III

TouchGFX derives the screen resolution from the LTDC interface setup. if you change it there it should change for the TouchGFX as well.

Ebun.1
Senior

Hello HP's

OK.

Thank you for your response.

Bob Bailey
Senior

Did this work? I will be doing a similar change soon.

I presume the LCD's ribbons are soldered to the Disco board (I have not looked). Did you install a connector?

Bob

There's no connector under the screen - it's soldered directly on the board. I've looked. Also, the connector is really wide, like 1mm pitch or similar, so soldering on a connector is not trivial.

Not tried yet.