‎2022-02-18 12:55 AM
Hi,
I have a custom board with STM32H7A3 using FMC, LLTC and other modules. I started to develop the firmware to change some images in a display. I made one project on TouchGFX with multiple images and fonts. I verify the BitmapDatabase.cpp and the all images files generated. For each image file generated for example:
LOCATION_PRAGMA("ExtFlashSection")
KEEP extern const unsigned char image_attention_all[] LOCATION_ATTRIBUTE("ExtFlashSection") = { // 223x265 RGB888 pixels.
0x0b, 0xba, 0xf7, 0x0b, 0xba, 0xf7, 0x0b, 0xba, 0xf7, 0x0b, 0xba, 0xf7,
...
...}
In my application.ld file I put that configurations that I view on https://support.touchgfx.com/4.18/docs/development/scenarios/using-non-memory-mapped-flash
/* Specify the memory areas */
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 1024K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
FLASH1 (rx) : ORIGIN = 0x8000000, LENGTH = 512K
FLASH2 (rx) : ORIGIN = 0x8100000, LENGTH = 512K
NOR1 (rx) : ORIGIN = 0x60000000, LENGTH = 64M /*External NOR Memory*/
SRAM (xrw) : ORIGIN = 0x62000000, LENGTH = 4M /*External SRAM Memory*/
}
.ARM.attributes 0 : { *(.ARM.attributes) }
ExtFlashSection :
{
*(ExtFlashSection ExtFlashSection.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >NOR1
FontFlashSection :
{
*(FontFlashSection FontFlashSection.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >NOR1
TextFlashSection :
{
*(TextFlashSection TextFlashSection.*)
*(.gnu.linkonce.r.*)
. = ALIGN(0x4);
} >NOR1
When I try to build the program I have section output from compiler:
What I'm doing wrong?
I only can write some program inside NOR1 when I change part of linker like:
/*Original data without write anything on NOR
/* Constant data goes into FLASH
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.)
*(.rodata*) /* .rodata* sections (constants, strings, etc.)
. = ALIGN(4);
} >FLASH1
*/
/* Constant data goes into FLASH */
.rodata :
{
. = ALIGN(4);
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
. = ALIGN(4);
} >NOR1
What am I doing wrong? How can I have a sure that I write all images files in External Flash?
Best regards,
Luis Cristovao
Solved! Go to Solution.
‎2022-02-18 5:30 AM
Your one image have around 170kB and isnt on any area linked, then error is in your makefile.
‎2022-02-18 5:01 AM
Are youy sure, that build is over images cpp files ?
And i see one problem
NOR1 (rx) : ORIGIN = 0x60000000, LENGTH = 64M /*External NOR Memory*/
SRAM (xrw) : ORIGIN = 0x62000000, LENGTH = 4M /*External SRAM Memory*/
64M ends override SRAM section +32M
‎2022-02-18 5:12 AM
Thanks for your reply MM..1
This morning I verify that SRAM need to be ORIGIN=0x64000000.
I think that I have the correct setting to build the project. I use Visual Studio Code with arm-none-eabi-gcc MakeFile . I add all images files (.cpp) generated by TouchGFX to my CmakeList.
What do you mean build is over images cpp files? Sorry because I never worked before with this type of architecture, I only worked before with microcontrollers PIC32.
Best regards, Luis
‎2022-02-18 5:18 AM
Thanks for your reply MM..1
This morning I verify that SRAM need to be ORIGIN=0x64000000.
I think that I have the correct setting to build the project. I use Visual Studio Code with arm-none-eabi-gcc MakeFile . I add all images files (.cpp) generated by TouchGFX to my CmakeList.
What do you mean build is over images cpp files? Sorry because I never worked before with this type of architecture, I only worked before with microcontrollers PIC32.
Best regards, Luis
‎2022-02-18 5:30 AM
Your one image have around 170kB and isnt on any area linked, then error is in your makefile.
‎2022-02-18 5:42 AM
What type of error? Can be anything with flags that I used?
I have this code CMakeList.txt:
cmake_minimum_required(VERSION 3.10)
# This is due to cross-compiling C/C++
set(CMAKE_TRY_COMPILE_TARGET_TYPE "STATIC_LIBRARY")
project(project C CXX ASM)
set(CMAKE_C_STANDARD 99)
set(CMAKE_CXX_STANDARD 17)
set(FREERTOS_ENABLE 1)
set(FREERTOS_HEAP_TYPE 4)
set(CMSIS_RTOS_VERSION 2)
add_executable(project_target_elf
TouchGFX/App/app_touchgfx.c
TouchGFX/generated/gui_generated/src/containers/Safe_ModeBase.cpp
TouchGFX/generated/gui_generated/src/containers/Normal_ModeBase.cpp
TouchGFX/generated/gui_generated/src/containers/Attention_ModeBase.cpp
TouchGFX/generated/gui_generated/src/containers/TopBarBase.cpp
TouchGFX/generated/gui_generated/src/mainscrenn_screen/MainScrennViewBase.cpp
TouchGFX/generated/gui_generated/src/common/FrontendApplicationBase.cpp
TouchGFX/gui/src/containers/Attention_Mode.cpp
TouchGFX/gui/src/containers/Normal_Mode.cpp
TouchGFX/gui/src/containers/TopBar.cpp
TouchGFX/gui/src/containers/Safe_Mode.cpp
TouchGFX/target/generated/STM32DMA.cpp
TouchGFX/target/generated/OSWrappers.cpp
TouchGFX/target/generated/TouchGFXConfiguration.cpp
TouchGFX/target/generated/TouchGFXGeneratedHAL.cpp
TouchGFX/target/TouchGFXHAL.cpp
TouchGFX/target/STM32TouchController.cpp
TouchGFX/target/TouchGFXGPIO.cpp
TouchGFX/target/generated/STM32DMA.cpp
TouchGFX/target/generated/OSWrappers.cpp
TouchGFX/target/TouchGFXGPIO.cpp
TouchGFX/gui/src/mainscrenn_screen/MainScrennView.cpp
TouchGFX/gui/src/mainscrenn_screen/MainScrennPresenter.cpp
TouchGFX/gui/src/common/FrontendApplication.cpp
TouchGFX/gui/src/model/Model.cpp
TouchGFX/generated/images/src/image_Attention.cpp
TouchGFX/generated/images/src/image_Attention_all.cpp
Core/Src/main.c
Core/Src/stm32h7xx_it.c
Core/Src/stm32h7xx_hal_msp.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_adc.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_adc_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_rcc_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_flash_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_gpio.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_hsem.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dma.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_dma_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_mdma.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pwr.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_pwr_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_cortex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_i2c.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_i2c_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_exti.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_crc.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_crc_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_fdcan.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_ll_fmc.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_nor.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_sram.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_ltdc.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_ltdc_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_tim_ex.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_uart.c
Drivers/STM32H7xx_HAL_Driver/Src/stm32h7xx_hal_uart_ex.c
Core/Src/system_stm32h7xx.c
Core/Src/freertos.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/croutine.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/event_groups.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/list.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/queue.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/stream_buffer.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/tasks.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/timers.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/CMSIS_RTOS_V2/cmsis_os2.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/portable/MemMang/heap_4.c
../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/portable/GCC/ARM_CM4F/port.c
Core/Src/stm32h7xx_hal_timebase_tim.c
target/startup/startup_stm32h7a3xx.s
)
target_include_directories(project_target_elf
PRIVATE
${CMAKE_CURRENT_SOURCE_DIR}/Middlewares/ST/touchgfx
${CMAKE_CURRENT_SOURCE_DIR}/Middlewares/ST/touchgfx/framework/include
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/App/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/target/generated/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/target/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/gui/include
${CMAKE_CURRENT_SOURCE_DIR}/Core/Inc/
${CMAKE_CURRENT_SOURCE_DIR}/Drivers/STM32H7xx_HAL_Driver/Inc/
${CMAKE_CURRENT_SOURCE_DIR}/Drivers/STM32H7xx_HAL_Driver/Inc/Legacy/
${CMAKE_CURRENT_SOURCE_DIR}/Drivers/CMSIS/Device/ST/STM32H7xx/Include/
${CMAKE_CURRENT_SOURCE_DIR}/Drivers/CMSIS/Include/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/gui_generated/include/gui_generated/containers
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/gui_generated/include/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/gui_generated/include/gui_generated/mainscrenn_screen
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/gui_generated/images/include
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/fonts/include/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/gui_generated/include/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/images/include/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/texts/include/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/generated/videos/include/
${CMAKE_CURRENT_SOURCE_DIR}/TouchGFX/gui/include/
${CMAKE_CURRENT_SOURCE_DIR}/../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/CMSIS_RTOS_V2
${CMAKE_CURRENT_SOURCE_DIR}/../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/include
${CMAKE_CURRENT_SOURCE_DIR}/../../../../submodules/stm/stm32h7/Middlewares/Third_Party/stm32_mw_freertos/Source/portable/GCC/ARM_CM4F
)
set_target_properties(project_target_elf PROPERTIES OUTPUT_NAME "project_target")
set_target_properties(project_target_elf PROPERTIES SUFFIX ".elf")
target_compile_options(project_target_elf
PRIVATE
-Wextra
-Wall
-pedantic
-Wno-unused
-Werror=implicit-function-declaration
)
add_subdirectory(../../../../submodules/asglobal/c/ deps/asglobal/)
add_subdirectory(../../../../submodules/stm/stm32h7 deps/vendor/stm)
target_include_directories(stm32h7xx_hal_driver
PRIVATE
${CMAKE_CURRENT_SOURCE_DIR}/Core/Inc/
)
target_include_directories(stm32_mw_freertos
PRIVATE
${CMAKE_CURRENT_SOURCE_DIR}/Core/Inc/
${CMAKE_CURRENT_SOURCE_DIR}/tracealyzer/Inc/
)
target_compile_definitions(project_target_elf
PRIVATE
-DMCPU
-DUSE_HAL_DRIVER
)
target_link_options(project_target_elf
PUBLIC
-Wl,-Map=${CMAKE_CURRENT_SOURCE_DIR}/target/mapfile.txt
-T${CMAKE_CURRENT_SOURCE_DIR}/target/application.ld
)
add_custom_command(
OUTPUT project_target.hex
COMMAND arm-none-eabi-objcopy -O ihex project_target.elf project_target.hex
DEPENDS project_target_elf
COMMENT "Creating hex file"
VERBATIM
)
add_custom_command(
OUTPUT project_target.bin
COMMAND arm-none-eabi-objcopy -O binary project_target.elf project_target.bin
DEPENDS project_target_elf
COMMENT "Creating binary file"
VERBATIM
)
add_custom_target(project_target ALL
COMMAND arm-none-eabi-size project_target.elf
DEPENDS project_target_elf
DEPENDS project_target.hex
DEPENDS project_target.bin
)
And the Cmake file have:
set(CMAKE_SYSTEM_NAME Generic)
set(CMAKE_SYSTEM_PROCESSOR arm)
set(CMAKE_C_COMPILER "arm-none-eabi-gcc.exe")
set(CMAKE_C_FLAGS
"-mthumb -mcpu=cortex-m7 -mfloat-abi=hard -mfpu=fpv5-d16 -DSTM32H7A3xx -DSTM32H7A3xx -fmessage-length=0 -ffunction-sections"
)
set(CMAKE_CXX_FLAGS
"-mthumb -mcpu=cortex-m7 -mfloat-abi=hard -mfpu=fpv5-d16 -DSTM32H7A3xx -DSTM32H7A3xx -fmessage-length=0 -ffunction-sections"
)
set(CMAKE_EXE_LINKER_FLAGS
"-mthumb -mcpu=cortex-m7 -mfloat-abi=hard -mfpu=fpv5-d16 --specs=nosys.specs -specs=nano.specs -Wl,--print-memory-usage -Wl,--gc-sections -Wl,--unresolved-symbols=ignore-in-object-files"
)
set(CMAKE_C_FLAGS_DEBUG "-O0 -g3")
set(CMAKE_C_FLAGS_RELEASE "-O3 -g0")
set(CMAKE_FIND_ROOT_PATH_MODE_PROGRAM NEVER)
set(CMAKE_FIND_ROOT_PATH_MODE_LIBRARY ONLY)
set(CMAKE_FIND_ROOT_PATH_MODE_INCLUDE ONLY)
set(CMAKE_FIND_ROOT_PATH_MODE_PACKAGE ONLY)
Thanks for your help.
‎2022-02-18 6:01 AM
here miss BitmapDatabase.cpp maybe more
i dont help you i preffer IDE or KEIL
‎2022-02-18 6:04 AM
I tried before with BitmapDatabase.cpp and the size of program don't change. Thanks for your help, I try to search more about it.
‎2022-02-18 6:41 AM
Thanks MM1, I solved my problem looking to the problem with other ideas.
The problem that I don't have any compiler to build .cpp files.
set(CMAKE_C_COMPILER "arm-none-eabi-gcc.exe")
set(CMAKE_CXX_COMPILER "arm-none-eabi-g++.exe")
Thanks a lot for your help :grinning_face:
‎2022-02-20 10:55 AM
My first linetip ... Are you sure, that build is over images cpp files ?
Marks some as Best reply for mark thread as solved...